Hello, I’m using Zed 2i Camera.
I used the camera to save RGB images, depth images, and point clouds.
In documentation, RGB, Depth images are load using Mat.read().
I checked the documentation, but there is no way to load the saved Point Cloud Value.
If my understanding is correct, the retrieve_measure and get value(x,y) functions are available when the camera is connected.
I want to detect the point cloud corresponding to the x and y coordinates of the image using the saved rgb, depth image, and point cloud file without connecting a camera.
I used python 3.7, Zed SDK 3.7, CUDA 11.5.
Thank you.