hello
I currently capture cows with a zed camera connected to a pc located on the farm and send RGB data (.png) and depth data (.pgm) to the central server.
However, this would require 1 pc with gpu for each zed camera.
So the price is a bit daunting.
Is there any way to capture images from the left and right lenses with zed camera one by one, send them to the central server, and infer the depth through the zed sdk api in the central server?
in void __cdecl sl::Mat::alloc(unsigned __int64,unsigned __int64,enum sl::MAT_TYPE,enum sl::MEM) : Err [999]: unknown error. NO GPU DETECTED
CUDA error at Camera.cpp:121 code=999(cudaErrorUnknown) “void __cdecl sl::close(void)”
CUDA error at Camera.cpp:149 code=999(cudaErrorUnknown) “void __cdecl sl::close(void)”
CUDA error at Camera.cpp:174 code=999(cudaErrorUnknown) “void __cdecl sl::close(void)”
CUDA error at Camera.cpp:214 code=999(cudaErrorUnknown) “void __cdecl sl::close(void)”
CUDA error at Camera.cpp:219 code=999(cudaErrorUnknown) “void __cdecl sl::close(void)”
CUDA error at sl_zed/CameraUtils.hpp:773 code=999(cudaErrorUnknown) “void __cdecl sl::ObjectsDetectorHandler::clear(void)”
CUDA error at sl_zed/CameraUtils.hpp:789 code=999(cudaErrorUnknown) “void __cdecl sl::ObjectsDetectorHandler::clear(void)”
CUDA error at sl_zed/CameraUtils.hpp:795 code=999(cudaErrorUnknown) “void __cdecl sl::ObjectsDetectorHandler::clear(void)”
CUDA error at sl_zed/CameraUtils.hpp:798 code=999(cudaErrorUnknown) “void __cdecl sl::ObjectsDetectorHandler::clear(void)”
CUDA error at sl_zed/CameraUtils.hpp:800 code=999(cudaErrorUnknown) “void __cdecl sl::ObjectsDetectorHandler::clear(void)”
CUDA error at sl_zed/CameraUtils.hpp:809 code=999(cudaErrorUnknown) “void __cdecl sl::ObjectsDetectorHandler::clear(void)”
CUDA error at Camera.cpp:234 code=999(cudaErrorUnknown) “void __cdecl sl::close(void)”
It was not possible to save svo file with python api in virtual environment.
However, if I connect the camera through the zed explorer program, it works without any problems, and I can save the svo file.
may i know what is the problem?
As per your advice, I would like to save only one frame as an svo file with python code and send it to the central server.