I executed the calibration between two cameras and got the intrinsic and extrinsic parameters.
My problem is that the extrinsic parameters are in the [R | T] matrix format (3x4):
[r1 r2 r3 t1;
r4 r5 r6 t2;
r7 r8 r9 t3;]
and I need the extrinsic parameters in the same format of the ZED calibration parameters file (.conf).
So, I need to extract from this matrix the Baseline, TY, TZ, RX_HD, CV_HD and RZ_HD parameters to add these values on the [STEREO] section of a ZED calibration file.
I would appreciate some help in how can I extract these values from the extrinsic matrix.