I Use the Sender To Send Data To Unreal By Zed livelink Plugin,but i can only got body animation data, in the source code :FrameData.cpp,i’ve found the camera data,but it’ll never change after i add the livelink source. the body data will change when i do the same thing.
Hi,
Yes the plugin can also send some additional data such as the camera position.
If the position never changes, can you verify in the configuration file the “set_as_static” parameter is not set to true?