Hello, when I was using zed, I met the following problems, they have been bothering me for a long time, could you please help me try to solve them?

Hello, when I was using zed, I met the following problems, they have been bothering me for a long time, could you please help me try to solve them?

First problem, in the installation of zed-sdk, my installation location is: /usr/local/zed, in this directory there is a setting folder, in this folder there is a SN8452341.conf, after opening it will display the following data:

[LEFT_CAM_2K]
fx=1403.76
fy=1403.4
cx=1109.57
cy=592.367
k1=-0.175286
k2=0.0283094
p1=6.68414e-05
p2=-0.000150431
k3=4.06032e-11

[RIGHT_CAM_2K]
fx=1401.93
fy=1402.22
cx=1094.03
cy=622.627
k1=-0.172795
k2=0.0265223
p1=0.000164482
p2=1.02174e-05
k3=-1.0484e-10

[LEFT_CAM_FHD]
fx=1403.76
fy=1403.4
cx=965.57
cy=511.367
k1=-0.175286
k2=0.0283094
p1=6.68414e-05
p2=-0.000150431
k3=4.06032e-11

[RIGHT_CAM_FHD]
fx=1401.93
fy=1402.22
cx=950.03
cy=541.627
k1=-0.172795
k2=0.0265223
p1=0.000164482
p2=1.02174e-05
k3=-1.0484e-10

[LEFT_CAM_HD]
fx=701.88
fy=701.7
cx=641.285
cy=344.1835
k1=-0.175286
k2=0.0283094
p1=6.68414e-05
p2=-0.000150431
k3=4.06032e-11

[RIGHT_CAM_HD]
fx=700.965
fy=701.11
cx=633.515
cy=359.3135
k1=-0.172795
k2=0.0265223
p1=0.000164482
p2=1.02174e-05
k3=-1.0484e-10

[LEFT_CAM_VGA]
fx=350.94
fy=350.85
cx=336.1425
cy=179.59175
k1=-0.175286
k2=0.0283094
p1=6.68414e-05
p2=-0.000150431
k3=4.06032e-11

[RIGHT_CAM_VGA]
fx=350.4825
fy=350.555
cx=332.2575
cy=187.15675
k1=-0.172795
k2=0.0265223
p1=0.000164482
p2=1.02174e-05
k3=-1.0484e-10

[STEREO]
Baseline=119.978
TY=0.0259812
TZ=0.0158877
CV_2K=0.00623976
CV_FHD=0.00623976
CV_HD=0.00623976
CV_VGA=0.00623976
RX_2K=-0.000916611
RX_FHD=-0.000916611
RX_HD=-0.000916611
RX_VGA=-0.000916611
RZ_2K=0.000770041
RZ_FHD=0.000770041
RZ_HD=0.000770041
RZ_VGA=0.000770041

[MISC]
Sensor_ID=0

What does this data mean, in particular RIGHT_CAM_VGA, RIGHT_CAM_HD, RIGHT_CAM_FHD], TY, TZ and V_FHD, RX_FHD, RZ_FHD and so on? In addition, in the SN8452341.conf file, what is the relationship between these parameters and the rotation matrix R and the translation matrix T between the two cameras? If there is a relationship, please use the data here to help me show it, thank you!

The second question is: how is the camera coordinate system of zed camera established? I used the zed data in zed_ros_wrapper package and found that the positive direction of x axis is the vertical mirror facing out, the positive direction of z axis is parallel to the mirror facing up, and the positive direction of y axis is parallel to the mirror from the left eye to the right eye. Is this coordinate axis correct? As shown in the picture below:

There is one last question: After a pixel coordinate (U, V) has been calibrated to obtain the corresponding parameter, can the correct three-dimensional coordinate be obtained through the following code? Please help me answer: Thank you!

#https://blog.csdn.net/qq_45077760/article/details/130091375?spm=1001.2014.3001.5502

import sys
import cv2
import numpy as np

# Binocular camera parameter
class stereoCamera(object):
    def __init__(self):
        # Left camera parameters
        self.cam_matrix_left = np.array([   [479.6018,   -0.0769,  652.6060],
                                            [       0,  478.0229,  352.3870],
                                            [       0,         0,         1]
                                        ])
        # Right camera parameters
        self.cam_matrix_right = np.array([  [489.9354,   0.2789,  641.6219],
                                            [       0,  487.9356,  354.5612],
                                            [       0,         0,         1]
                                        ])

        # Left and right camera distortion factor:[k1, k2, p1, p2, k3]
        self.distortion_l = np.array([[-0.0791, 0.0309, -0.0009, -0.0004, -0.0091]])
        self.distortion_r = np.array([[-0.1153, 0.1021, -0.0011,  -0.0005,  -0.0459]])

        # Right camera translation matrix and rotation matrix relative to left camera
        # Rotation matrix
        self.R = np.array([ [1.0000,  0.0005, -0.0184],
                            [-0.0005,  1.0000, 0.0001],
                            [ 0.0184,  -0.0001,  1.0000]
                            ])
        # Translation matrix

        self.T = np.array([[121.4655], [0.2118], [0.5950]])
        # Focus Distance
        self.focal_length = 749.402  #The default value is generally Q in the stereocorrected reprojection matrix Q[2,3].
        # Baseline distance
        self.baseline = 121.4655  # Unit: mm, the first parameter of the translation vector (absolute value)



# preconditioning
def preprocess(img1, img2):
    # Color image -> Grayscale image
    if (img1.ndim == 3):  # Determine whether it is a three-dimensional array
        img1 = cv2.cvtColor(img1, cv2.COLOR_BGR2GRAY)  # Convert from BGR color space to grayscale image.
    if (img2.ndim == 3):
        img2 = cv2.cvtColor(img2, cv2.COLOR_BGR2GRAY)

    #Histogram equalization
    # Histogram equalization is an image enhancement technique, which can improve the contrast of the image and make the distribution of pixel values in the image more uniform.
    # In image processing, histogram equalization is often used to improve image brightness and contrast, especially in lighting
    img1 = cv2.equalizeHist(img1)
    img2 = cv2.equalizeHist(img2)

    return img1, img2


# Distortion elimination
# Function returns a dedistorted image
#
# image:The input image is usually a color image
# c

Hi @daiwei125
you should not use the calibration file to retrieve the camera parameters.
The calibration files contains information relative to the unrectified images and the ZED SDK performs a self-recalibration when it starts.

You can obtain all the information that you are searching for by using the ZED SDK API:

Regarding the camera coordinate system, if you are not using ROS, you should not look at it, but read the Stereolabs documentation.
The coordinate system reflects the setting that you use for InitParameters::coordinate_system → Core Module | API Reference | Stereolabs