GMSL driver installation issue on AVerMedia D315 carrier board

Hello,

I am trying to use the ZED X Mini by connecting a GMSL2 board to AVerMedia’s D315 carrier board.
When I try to install the ZED camera driver provided on the ZED website, I get an error saying that the kernel version is not compatible, and the installation fails.

Currently, I am using JetPack 6.0, and I believe the issue is caused by a slight difference between the kernel version of the carrier board and the original kernel version of JetPack 6.0.

I would like to know if ZED can provide a camera driver that is compatible with the AVerMedia D315 board running JetPack 6.0.
If not, I would appreciate any suggestions or alternative solutions.

Hi @wonnerky
Welcome to the Stereolabs community.

Please contact AVerMedia to obtain the latest available driver that they released.

Hi @Myzhar
Thank you for your response. What I meant was that the driver from the link below cannot be installed on the AVerMedia carrier board.
https://www.stereolabs.com/en-kr/developers/drivers
Is this driver also provided by AVerMedia?

Yes, it is. Please contact AVerMedia for more information.

Thank you for your help! :+1: