Git-sample multi-kamera multi-model not detecting anything (custom and sl)

Hello everyone,

i have four Zed X and at the moment i have the problem that i cant detect anything in fusion. I am using a Jetson AGX 64 GB and Stereolabs SDK 5.0.5. Single detection ist working aka. (tensorrt_internal). We can see us running around in the point cloud but there are no boxes. Prior 5.0.5 (4.x) it was working.

Did you changed something important in 5.0.5?

We also updated all code samples because of the restructure of some parameters in 5.0.5. This is already done.

Hi @DG_Ost
Welcome to the Stereolabs community.

Please update the ZED SDK to the latest v5.0.7.

I recommend you clean the /usr/local/zed folder before updating to remove any residual AI model optimization.

In case the problem persists, please share the code that you are using and eventually the custom AI models with SVO recording to try to reproduce the problem at our labs.

Hi @Myzhar ,

i am sorry for the late response, this had solved our problems.

Best Regards,

DG_Ost