How do I get the maximum depth measurement for a given Zed camera in python?
Hi @frigusgulo,
You can retrieve the maximum depth measurement for a ZED camera by leaving the default value to the initParameters object and retrieving it after opening the camera, as the camera model is determined when opening the camera.
import pyzed.sl as sl
def main():
# Create a Camera object
zed = sl.Camera()
# Initialize a Camera configuration
init_params = sl.InitParameters()
init_params.depth_mode = sl.DEPTH_MODE.PERFORMANCE
init_params.coordinate_units = sl.UNIT.CENTIMETER # Unit of measurement
# Open the camera
err = zed.open(init_params)
if err != sl.ERROR_CODE.SUCCESS:
exit(1)
print(f"Maximum Depth Range: {zed.get_init_parameters().depth_maximum_distance} centimeters")
# Close the camera
zed.close()
if __name__ == "__main__":
main()