Updated to 4.0.6!!
and continued working on getting fusion right but the issue I am facing is,
File “zed-sdk-master/tutorials/tutorial 9 - geotracking/python/geotracking.py”, line 83, in
fusion.enable_positionnal_tracking()
TypeError: enable_positionnal_tracking() takes exactly one argument (0 given)
same error with samples in geotracking too,
I tried inputting possitional tracking params in function as
“fusion.enable_positionnal_tracking(tracking_params)”
resulting in,
Traceback (most recent call last):
File “zed-sdk-master/tutorials/tutorial 9 - geotracking/python/geotracking.py”, line 83, in
fusion.enable_positionnal_tracking(tracking_params)
File “pyzed/sl.pyx”, line 10653, in pyzed.sl.Fusion.enable_positionnal_tracking
File “stringsource”, line 14, in FromPyStructUtility.__pyx_convert__from_py_struct__sl_3a__3a_PositionalTrackingFusionParameters
TypeError: Expected a mapping, got pyzed.sl.PositionalTrackingParameters
so, It requires “mapping” not the params, Stereolabs team can you please help me regarding this, I believe it has to do with newer 4.0.6 sdk because earlier in 4.0.5 it was working fine with this function although fusion has not worked for me til date.
ps: I can confirm the camera opens well n good so does the gnss module.
Traceback (most recent call last):
File "tracking.py", line 88, in <module>
fusion_tracking_params.gnss_calibration_parameters = sl.GNSSCalibrationParameters() #gnss_calibration_parameters
File "pyzed/sl.pyx", line 9858, in pyzed.sl.PositionalTrackingFusionParameters.gnss_calibration_parameters.__set__
File "stringsource", line 14, in FromPyStructUtility.__pyx_convert__from_py_struct__sl_3a__3a_GNSSCalibrationParameters
TypeError: Expected a mapping, got pyzed.sl.GNSSCalibrationParameters
Traceback (most recent call last):
File "tracking.py", line 90, in <module>
fusion.enable_positionnal_tracking(fusion_tracking_params)
File "pyzed/sl.pyx", line 10653, in pyzed.sl.Fusion.enable_positionnal_tracking
File "stringsource", line 14, in FromPyStructUtility.__pyx_convert__from_py_struct__sl_3a__3a_PositionalTrackingFusionParameters
TypeError: Expected a mapping, got pyzed.sl.PositionalTrackingFusionParameters