Gemini is suggesting to me that that the real issue with processing the kernel packages might be the contents of /etc/nv_boot_control.conf, and that I appear to have a generic version of that file rather than a Zed-specific version of that file. Is there a Zed-specific version that can be shared? (I have a Zed Box Orin 16GB). If so, the flashing script might need to be updated to install that file so that users don’t have to wipe the /var/lib/dpkg/info directory
There’s really nothing else in the error logs. Just thousands of lines complaining about the files list is missing from /var/lib/dpkg/info/ having been removed. I think I solved that issue, but I can’t get the camera to work anymore and I’m wondering if reinstalling all the packages messed something up and I need to reflash again.
The big question I still have is whether there’s anything Zed-specific that’s supposed to live in /etc/nv_boot_control.conf ?
I wonder if the directions on Flash your ZED Box Orin - Stereolabs are potentially out of order and if perhaps Update the System (Step 5) should come after Install ZED Link Drivers (Step 9). Because I think that updating the system might require /etc/nv_boot_control.conf to be correctly populated to identify the carrier board. I think the reason the /var/lib/dpkg/info/ directory needs to be blown away in the instructions might be as a workaround for that file not having been updated yet.