Exporting IMU and Point Cloud from Loaded SVO File:
I am working with a ZED2 camera using ROS Noetic on Ubuntu 20.04 in WSL. My laptop is a Dell Precision 7530 Mobile Workstation (Intel Core i7, 64GB RAM, Nvidia Quadro P2000 – compute capability 6.1). I am using ZED_SDK_Ubuntu20_cuda12.1_v4.0.8.zstd.run.
I would like to inquire about how to export/publish a topic from a loaded SVO file. When I use zed_wrapper, it does not create a BAG file. During processing, a warning is displayed:
‘[2023-12-30 07:06:35 UTC][ZED][WARNING] END OF SVO FILE REACHED in sl::ERROR_CODE sl:
:grab(sl::RuntimeParameters)’
I have tried two SVO files with the same result. Both files can be played in the ZED Explorer.
roslaunch zed_wrapper zed2.launch svo_file:=HD720_SN20817774_10-03-38.svo
I would like to obtain IMU data and a point cloud. I can export frames in the SDK under Windows using ZED_SVO_Export (without losing frames). Is there a way to export these topics (IMU, point cloud) from an existing SVO file, or does it need to be addressed during recording? What is the issue with creating a bag file, and which configuration files need to be modified?
Thank you for any assistance.
roslaunch zed_wrapper zed2.launch svo_file:=HD720_SN20817774_10-03-38.svo
Here are the parameters when running the above command:
SUMMARY
PARAMETERS
- /rosdistro: noetic
- /rosversion: 1.16.0
- /zed2/zed2_description: <?xml version="1…
- /zed2/zed_node/auto_exposure_gain: True
- /zed2/zed_node/auto_whitebalance: True
- /zed2/zed_node/brightness: 4
- /zed2/zed_node/contrast: 4
- /zed2/zed_node/depth/depth_mode: ULTRA
- /zed2/zed_node/depth/depth_stabilization: 1
- /zed2/zed_node/depth/max_depth: 15.0
- /zed2/zed_node/depth/min_depth: 0.3
- /zed2/zed_node/depth/openni_depth_mode: False
- /zed2/zed_node/depth_confidence: 50
- /zed2/zed_node/depth_texture_conf: 100
- /zed2/zed_node/exposure: 100
- /zed2/zed_node/gain: 100
- /zed2/zed_node/gamma: 8
- /zed2/zed_node/general/base_frame: base_link
- /zed2/zed_node/general/camera_flip: AUTO
- /zed2/zed_node/general/camera_model: zed2
- /zed2/zed_node/general/camera_name: zed2
- /zed2/zed_node/general/gpu_id: -1
- /zed2/zed_node/general/grab_frame_rate: 30
- /zed2/zed_node/general/grab_resolution: HD720
- /zed2/zed_node/general/pub_downscale_factor: 2.0
- /zed2/zed_node/general/pub_frame_rate: 15.0
- /zed2/zed_node/general/pub_resolution: CUSTOM
- /zed2/zed_node/general/region_of_interest:
- /zed2/zed_node/general/sdk_verbose: 1
- /zed2/zed_node/general/self_calib: True
- /zed2/zed_node/general/serial_number: 0
- /zed2/zed_node/general/svo_compression: 2
- /zed2/zed_node/general/svo_realtime: True
- /zed2/zed_node/general/zed_id: 0
- /zed2/zed_node/hue: 0
- /zed2/zed_node/mapping/clicked_point_topic: /clicked_point
- /zed2/zed_node/mapping/fused_pointcloud_freq: 1.0
- /zed2/zed_node/mapping/mapping_enabled: False
- /zed2/zed_node/mapping/max_mapping_range: -1
- /zed2/zed_node/mapping/resolution: 0.05
- /zed2/zed_node/object_detection/allow_reduced_precision_inference: True
- /zed2/zed_node/object_detection/max_range: 15.0
- /zed2/zed_node/object_detection/mc_animal: True
- /zed2/zed_node/object_detection/mc_bag: True
- /zed2/zed_node/object_detection/mc_electronics: True
- /zed2/zed_node/object_detection/mc_fruit_vegetable: True
- /zed2/zed_node/object_detection/mc_people: True
- /zed2/zed_node/object_detection/mc_sport: True
- /zed2/zed_node/object_detection/mc_vehicle: True
- /zed2/zed_node/object_detection/model: MULTI_CLASS_BOX_A…
- /zed2/zed_node/object_detection/object_tracking_enabled: True
- /zed2/zed_node/object_detection/od_enabled: False
- /zed2/zed_node/object_detection/prediction_timeout: 0.5
- /zed2/zed_node/point_cloud_freq: 10.0
- /zed2/zed_node/pos_tracking/area_memory: True
- /zed2/zed_node/pos_tracking/area_memory_db_path:
- /zed2/zed_node/pos_tracking/depth_min_range: 0.0
- /zed2/zed_node/pos_tracking/fixed_z_value: 0.0
- /zed2/zed_node/pos_tracking/floor_alignment: False
- /zed2/zed_node/pos_tracking/imu_fusion: True
- /zed2/zed_node/pos_tracking/init_odom_with_first_valid_pose: True
- /zed2/zed_node/pos_tracking/initial_base_pose: [0.0, 0.0, 0.0, 0…
- /zed2/zed_node/pos_tracking/map_frame: map
- /zed2/zed_node/pos_tracking/odometry_frame: odom
- /zed2/zed_node/pos_tracking/path_max_count: -1
- /zed2/zed_node/pos_tracking/path_pub_rate: 2.0
- /zed2/zed_node/pos_tracking/pos_tracking_enabled: True
- /zed2/zed_node/pos_tracking/pos_tracking_mode: STANDARD
- /zed2/zed_node/pos_tracking/publish_map_tf: True
- /zed2/zed_node/pos_tracking/publish_tf: True
- /zed2/zed_node/pos_tracking/save_area_memory_db_on_exit: False
- /zed2/zed_node/pos_tracking/set_as_static: False
- /zed2/zed_node/pos_tracking/set_gravity_as_origin: True
- /zed2/zed_node/pos_tracking/two_d_mode: False
- /zed2/zed_node/saturation: 4
- /zed2/zed_node/sensors/max_pub_rate: 400.0
- /zed2/zed_node/sensors/publish_imu_tf: True
- /zed2/zed_node/sensors/sensors_timestamp_sync: False
- /zed2/zed_node/sharpness: 4
- /zed2/zed_node/stream:
- /zed2/zed_node/svo_file: HD720_SN20817774_…
- /zed2/zed_node/whitebalance_temperature: 42
NODES
/zed2/
zed2_state_publisher (robot_state_publisher/robot_state_publisher)
zed_node (zed_wrapper/zed_wrapper_node)
auto-starting new master
process[master]: started with pid [1148]
ROS_MASTER_URI=http://localhost:11311
setting /run_id to 068c4f8e-a6df-11ee-a422-7bb975a7085e
process[rosout-1]: started with pid [1169]
started core service [/rosout]
process[zed2/zed2_state_publisher-2]: started with pid [1172]
process[zed2/zed_node-3]: started with pid [1173]
[ INFO] [1703918734.380614457]: Initializing nodelet with 12 worker threads.
[ INFO] [1703918734.767902570]: ********** Starting nodelet ‘/zed2/zed_node’ **********
[ INFO] [1703918734.767999870]: SDK version: 4.0.8
[ INFO] [1703918734.772707570]: *** GENERAL PARAMETERS ***
[ INFO] [1703918734.773452670]: * Camera Model by param → zed2
[ INFO] [1703918734.774099070]: * Camera Name → zed2
[ INFO] [1703918734.774613570]: * Camera resolution → HD720
[ INFO] [1703918734.775116470]: * Camera Grab Framerate → 30
[ INFO] [1703918734.775671470]: * Grab compute capping FPS → 15 Hz
[ INFO] [1703918734.776217370]: * Publishing resolution → CUSTOM
[ INFO] [1703918734.776746270]: * Publishing downscale factor → 2
[ INFO] [1703918734.777182370]: * Gpu ID → -1
[ INFO] [1703918734.777696270]: * Camera ID → 0
[ INFO] [1703918734.778385070]: * SDK Verbose level → 1
[ INFO] [1703918734.779239870]: * Camera Flip → AUTO
[ INFO] [1703918734.779834270]: * Self calibration → ENABLED
[ INFO] [1703918734.780847670]: * Region of interest →
[ INFO] [1703918734.780928270]: *** DEPTH PARAMETERS ***
[ INFO] [1703918734.781706370]: * Depth mode → ULTRA [3]
[ INFO] [1703918734.782228770]: * OpenNI mode → DISABLED
[ INFO] [1703918734.782651770]: * Depth Stabilization → 1
[ INFO] [1703918734.783065770]: * Minimum depth → 0.3 m
[ INFO] [1703918734.783475370]: * Maximum depth → 15 m
[ INFO] [1703918734.783531370]: *** POSITIONAL TRACKING PARAMETERS ***
[ INFO] [1703918734.783951770]: * Positional tracking → ENABLED
[ INFO] [1703918734.784488070]: * Positional tracking mode → POSITIONAL TRACKING MODE STANDARD
[ INFO] [1703918734.784975570]: * Set gravity as origin → ENABLED
[ INFO] [1703918734.785429670]: * Path rate → 2 Hz
[ INFO] [1703918734.785917770]: * Path history size → 1
[ INFO] [1703918734.786606670]: * Odometry DB path →
[ INFO] [1703918734.786979170]: * Save Area Memory on closing → DISABLED
[ INFO] [1703918734.787781070]: * Area Memory → ENABLED
[ INFO] [1703918734.788262170]: * IMU Fusion → ENABLED
[ INFO] [1703918734.788646470]: * Floor alignment → DISABLED
[ INFO] [1703918734.789081671]: * Init Odometry with first valid pose data → ENABLED
[ INFO] [1703918734.789467671]: * Force 2D mode → DISABLED
[ INFO] [1703918734.789927071]: * Broadcast odometry TF → ENABLED
[ INFO] [1703918734.790397171]: * Broadcast map pose TF → ENABLED
[ INFO] [1703918734.790900171]: * Camera is static → DISABLED
[ INFO] [1703918734.791399871]: * Depth minimum range → 0
[ INFO] [1703918734.791477571]: *** MAPPING PARAMETERS ***
[ INFO] [1703918734.792001571]: * Mapping → DISABLED
[ INFO] [1703918734.792819771]: * Clicked point topic → /clicked_point
[ INFO] [1703918734.792953571]: *** OBJECT DETECTION PARAMETERS ***
[ INFO] [1703918734.793687571]: * Object Detection → DISABLED
[ INFO] [1703918734.794807671]: * Object confidence → 50
[ INFO] [1703918734.795513071]: * Object tracking → ENABLED
[ INFO] [1703918734.796172471]: * Detection max range → 15
[ INFO] [1703918734.796659671]: * Allow reduced precision → ENABLED
[ INFO] [1703918734.797203571]: * Prediction Timeout → 0.5
[ INFO] [1703918734.797849571]: * Object Det. model ->MULTI CLASS BOX ACCURATE
[ INFO] [1703918734.798850571]: * Detect people → ENABLED
[ INFO] [1703918734.799766771]: * Detect vehicles → ENABLED
[ INFO] [1703918734.800458971]: * Detect bags → ENABLED
[ INFO] [1703918734.800911071]: * Detect animals → ENABLED
[ INFO] [1703918734.801320771]: * Detect electronics → ENABLED
[ INFO] [1703918734.801713371]: * Detect fruit and vegetables → ENABLED
[ INFO] [1703918734.802098571]: * Detect sport-related objects → ENABLED
[ INFO] [1703918734.802158171]: *** SENSORS PARAMETERS ***
[ INFO] [1703918734.802545771]: * Sensors timestamp sync → DISABLED
[ INFO] [1703918734.803023971]: * Max sensors rate → 400
[ INFO] [1703918734.803484271]: * Broadcast IMU pose TF → ENABLED
[ INFO] [1703918734.803592271]: *** SVO PARAMETERS ***
[ INFO] [1703918734.804524571]: * SVO input file: → /home/pavol/.ros/HD720_SN20817774_10-03-38.svo
[ INFO] [1703918734.804990471]: * SVO realtime mode → ENABLED
[ INFO] [1703918734.805526471]: * SVO REC compression → H265 (HEVC)
[ INFO] [1703918734.806135871]: *** COORDINATE FRAMES ***
[ INFO] [1703918734.807478971]: * camera_frame → zed2_camera_center
[ INFO] [1703918734.807538371]: * imu_link → zed2_imu_link
[ INFO] [1703918734.807630171]: * left_camera_frame → zed2_left_camera_frame
[ INFO] [1703918734.807682171]: * left_camera_optical_frame → zed2_left_camera_optical_frame
[ INFO] [1703918734.807755671]: * right_camera_frame → zed2_right_camera_frame
[ INFO] [1703918734.807812571]: * right_camera_optical_frame → zed2_right_camera_optical_frame
[ INFO] [1703918734.807864671]: * map_frame → map
[ INFO] [1703918734.807898671]: * odometry_frame → odom
[ INFO] [1703918734.807931471]: * base_frame → base_link
[ INFO] [1703918734.807992071]: * depth_frame → zed2_left_camera_frame
[ INFO] [1703918734.808151871]: * depth_optical_frame → zed2_left_camera_optical_frame
[ INFO] [1703918734.808244671]: * disparity_frame → zed2_left_camera_frame
[ INFO] [1703918734.808344571]: * disparity_optical_frame → zed2_left_camera_optical_frame
[ INFO] [1703918734.808434471]: * confidence_frame → zed2_left_camera_frame
[ INFO] [1703918734.808511471]: * confidence_optical_frame → zed2_left_camera_optical_frame
[ INFO] [1703918734.813483371]: * Camera coordinate system → Right HANDED Z UP and X FORWARD
[ INFO] [1703918734.813581371]: *** Opening ZED 2 - SVO - /home/pavol/.ros/HD720_SN20817774_10-03-38.svo ***
[2023-12-30 06:45:34 UTC][ZED][INFO] Logging level INFO
[2023-12-30 06:45:40 UTC][ZED][INFO] [Init] Depth mode: ULTRA
[2023-12-30 06:45:40 UTC][ZED][INFO] [Init] Serial Number: S/N 20817774
[ INFO] [1703918740.461701437]: ZED connection [SVO - /home/pavol/.ros/HD720_SN20817774_10-03-38.svo]: SUCCESS
[ INFO] [1703918742.466413292]: … ZED ready
[ INFO] [1703918742.466493192]: ZED SDK running on GPU #0
[ INFO] [1703918742.466994092]: Camera-IMU Transform:
563F8A28CB68
0.999990 0.003893 0.002349 -0.002000
-0.003887 0.999989 -0.002503 -0.023000
-0.002359 0.002494 0.999994 -0.002000
0.000000 0.000000 0.000000 1.000000
[ INFO] [1703918742.467056992]: * CAMERA MODEL → ZED 2
[ INFO] [1703918742.467073992]: * Serial Number: 20817774
[ INFO] [1703918742.500821993]: *** PUBLISHERS ***
[ INFO] [1703918742.920006504]: * Advertised on topic /zed2/zed_node/rgb/image_rect_color
[ INFO] [1703918742.920116304]: * Advertised on topic /zed2/zed_node/rgb/camera_info
[ INFO] [1703918742.943604505]: * Advertised on topic /zed2/zed_node/rgb_raw/image_raw_color
[ INFO] [1703918742.943676005]: * Advertised on topic /zed2/zed_node/rgb_raw/camera_info
[ INFO] [1703918742.970383506]: * Advertised on topic /zed2/zed_node/left/image_rect_color
[ INFO] [1703918742.970507206]: * Advertised on topic /zed2/zed_node/left/camera_info
[ INFO] [1703918742.995431206]: * Advertised on topic /zed2/zed_node/left_raw/image_raw_color
[ INFO] [1703918742.995510306]: * Advertised on topic /zed2/zed_node/left_raw/camera_info
[ INFO] [1703918743.018069007]: * Advertised on topic /zed2/zed_node/right/image_rect_color
[ INFO] [1703918743.018154107]: * Advertised on topic /zed2/zed_node/right/camera_info
[ INFO] [1703918743.043079208]: * Advertised on topic /zed2/zed_node/right_raw/image_raw_color
[ INFO] [1703918743.043155208]: * Advertised on topic /zed2/zed_node/right_raw/camera_info
[ INFO] [1703918743.067567708]: * Advertised on topic /zed2/zed_node/rgb/image_rect_gray
[ INFO] [1703918743.067641908]: * Advertised on topic /zed2/zed_node/rgb/camera_info
[ INFO] [1703918743.089155109]: * Advertised on topic /zed2/zed_node/rgb_raw/image_raw_gray
[ INFO] [1703918743.089236309]: * Advertised on topic /zed2/zed_node/rgb_raw/camera_info
[ INFO] [1703918743.112944009]: * Advertised on topic /zed2/zed_node/left/image_rect_gray
[ INFO] [1703918743.113017109]: * Advertised on topic /zed2/zed_node/left/camera_info
[ INFO] [1703918743.137391910]: * Advertised on topic /zed2/zed_node/left_raw/image_raw_gray
[ INFO] [1703918743.137475510]: * Advertised on topic /zed2/zed_node/left_raw/camera_info
[ INFO] [1703918743.160138011]: * Advertised on topic /zed2/zed_node/right/image_rect_gray
[ INFO] [1703918743.160221511]: * Advertised on topic /zed2/zed_node/right/camera_info
[ INFO] [1703918743.182084211]: * Advertised on topic /zed2/zed_node/right_raw/image_raw_gray
[ INFO] [1703918743.182166811]: * Advertised on topic /zed2/zed_node/right_raw/camera_info
[ INFO] [1703918743.206497012]: * Advertised on topic /zed2/zed_node/stereo/image_rect_color
[ INFO] [1703918743.231320513]: * Advertised on topic /zed2/zed_node/stereo_raw/image_raw_color
[ INFO] [1703918743.253624513]: * Advertised on topic /zed2/zed_node/depth/depth_registered
[ INFO] [1703918743.253891913]: * Advertised on topic /zed2/zed_node/depth/camera_info
[ INFO] [1703918743.255307213]: * Advertised on topic /zed2/zed_node/confidence/confidence_map
[ INFO] [1703918743.255895513]: * Advertised on topic /zed2/zed_node/disparity/disparity_image
[ INFO] [1703918743.256378113]: * Advertised on topic /zed2/zed_node/point_cloud/cloud_registered
[ INFO] [1703918743.256866113]: * Advertised on topic /zed2/zed_node/pose
[ INFO] [1703918743.257352213]: * Advertised on topic /zed2/zed_node/pose_with_covariance
[ INFO] [1703918743.257828513]: * Advertised on topic /zed2/zed_node/odom
[ INFO] [1703918743.258307413]: * Advertised on topic /zed2/zed_node/odom/status
[ INFO] [1703918743.259281113]: * Advertised on topic /zed2/zed_node/pose/status
[ INFO] [1703918743.261739414]: * Advertised on topic /zed2/zed_node/path_odom
[ INFO] [1703918743.262608114]: * Advertised on topic /zed2/zed_node/path_map
[ INFO] [1703918743.264031714]: * Advertised on topic /zed2/zed_node/imu/data
[ INFO] [1703918743.264887814]: * Advertised on topic /zed2/zed_node/imu/data_raw
[ INFO] [1703918743.265415814]: * Advertised on topic /zed2/zed_node/temperature/imu
[ INFO] [1703918743.265900014]: * Advertised on topic /zed2/zed_node/imu/mag
[ INFO] [1703918743.266342114]: * Advertised on topic /zed2/zed_node/atm_press
[ INFO] [1703918743.266848014]: * Advertised on topic /zed2/zed_node/temperature/left
[ INFO] [1703918743.267393014]: * Advertised on topic /zed2/zed_node/temperature/right
[ INFO] [1703918743.267904314]: * Advertised on topic /zed2/zed_node/left_cam_imu_transform [LATCHED]
[ INFO] [1703918743.267976614]: *** SUBSCRIBERS ***
[ INFO] [1703918743.270460714]: * Subscribed to topic /clicked_point
[ INFO] [1703918743.270539214]: *** SERVICES ***
[ INFO] [1703918743.270995814]: * Advertised on service /zed2/zed_node/set_pose
[ INFO] [1703918743.271439014]: * Advertised on service /zed2/zed_node/reset_odometry
[ INFO] [1703918743.271940514]: * Advertised on service /zed2/zed_node/reset_tracking
[ INFO] [1703918743.272451814]: * Advertised on service /zed2/zed_node/save_area_memory
[ INFO] [1703918743.273010714]: * Advertised on service /zed2/zed_node/start_3d_mapping
[ INFO] [1703918743.273563914]: * Advertised on service /zed2/zed_node/stop_3d_mapping
[ INFO] [1703918743.274169314]: * Advertised on service /zed2/zed_node/save_3d_map
[ INFO] [1703918743.274737714]: * Advertised on service /zed2/zed_node/enable_object_detection
[ INFO] [1703918743.275663714]: * Advertised on service /zed2/zed_node/start_svo_recording
[ INFO] [1703918743.276205014]: * Advertised on service /zed2/zed_node/stop_svo_recording
[ INFO] [1703918743.276805214]: * Advertised on service /zed2/zed_node/set_led_status
[ INFO] [1703918743.277300014]: * Advertised on service /zed2/zed_node/toggle_led
[ INFO] [1703918743.277750614]: * Advertised on service /zed2/zed_node/start_remote_stream
[ INFO] [1703918743.278198814]: * Advertised on service /zed2/zed_node/stop_remote_stream
[ INFO] [1703918743.278639114]: * Advertised on service /zed2/zed_node/set_roi
[ INFO] [1703918743.279082814]: * Advertised on service /zed2/zed_node/set_roi
[ INFO] [1703918743.279277014]: +++ ZED Node started +++
[ INFO] [1703918743.279388914]: Published static transform ‘zed2_imu_link’ → ‘zed2_left_camera_frame’
[ INFO] [1703918743.279550714]: *** Starting Positional Tracking ***
[ INFO] [1703918743.279626014]: * Waiting for valid static transformations…
[ INFO] [1703918743.279739014]: Static transform Sensor to Base [zed2_left_camera_frame → base_link]
[ INFO] [1703918743.279810914]: * Translation: {0.011,-0.060,-0.015}
[ INFO] [1703918743.279897014]: * Rotation: {0.000,-2.865,0.000}
[ INFO] [1703918743.279972114]: Static transform Sensor to Camera Center [zed2_left_camera_frame → zed2_camera_center]
[ INFO] [1703918743.280049614]: * Translation: {0.010,-0.060,0.000}
[ INFO] [1703918743.280094114]: * Rotation: {0.000,-0.000,0.000}
[ INFO] [1703918743.280172114]: Static transform Camera Center to Base [zed2_camera_center → base_link]
[ INFO] [1703918743.280238614]: * Translation: {0.001,0.000,-0.015}
[ INFO] [1703918743.280316214]: * Rotation: {0.000,-2.865,0.000}
[ INFO] [1703918743.780528728]: Initial ZED left camera pose (ZED pos. tracking):
[ INFO] [1703918743.780631428]: * T: [-0.0099875,0.06,0.0154998]
[ INFO] [1703918743.780739928]: * Q: [0,0.0249979,0,0.999687]