Error occurs when installing zedlink duo driver with jetpack 6.2.2

Version info:

Ubuntu: 22.04.5

L4T: 36.5

Jetpack: 6.2.2+b24

ZED SDK: 5.2.3

ZED driver: 1.4.2

Problem description:

Unable to start zed_x_daemon.service. Download from official release link: driver ; Install with dpkg; reboot after installation. In contrast, if extract the .deb file, and copy the files to corresponding directories, the ZED_Diagnostic will show that driver is not installed.

running sudo ZED_Diagnostic -c

The error info is in the attached json file;

Also try to activate zed_x_daemon: sudo systemctl enable zed_x_daemon driver_zed_loader IMU_Daemon

This is the result I got:

Failed to enable unit: Unit file zed_x_daemon.service does not exist.

I’d appreciate your reply.