I’m attempting to download the newest driver for Jetpack 6.x and I’m getting the following error:
$ sudo dpkg -i stereolabs-zedlink-duo_1.1.1-LI-MAX96712-L4T36.3.0_arm64.deb
[sudo] password for pack-user-cv:
dpkg: regarding stereolabs-zedlink-duo_1.1.1-LI-MAX96712-L4T36.3.0_arm64.deb containing stereolabs-zedlink-duo, pre-dependency problem: stereolabs-zedlink-duo pre-depends on nvidia-l4t-core (<< 36.4-0)
nvidia-l4t-core is installed, but is version 36.4.0-20240912212859.
dpkg: error processing archive stereolabs-zedlink-duo_1.1.1-LI-MAX96712-L4T36.3.0_arm64.deb (–install):
pre-dependency problem - not installing stereolabs-zedlink-duo
Errors were encountered while processing: stereolabs-zedlink-duo_1.1.1-LI-MAX96712-L4T36.3.0_arm64.deb
%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%
I’m not sure how to downgrade the l4t to 36.3. I attempted the debian based method to make the r36.4 to r36.3 but the error persists. Would like some insight on what to do.
Gave it an attempt but didn’t see an option for 36.3. The host computer is a 22.04, do I need a lower Ubuntu version to change it? Or am I missing something? Even the archived won’t show the other 36.3 version I am looking for.
Thanks again Walter for the continuous help
Best,
Ramon
I’ve installed JP 6.0 and now at L4T v36.3. I tried the multi_cam.py script as well as attempted to open two instances of ZED_Explorer, but I still can’t get the two cameras to work at the same time. The first camera that opens will function as expected but the second cameras always fails. I will include the diagnostic file here.
It’s whatever the sample script utilizes. But regardless when I open ZED_Explorer the first camera works, however in the same ZED_Explorer window, when I attempt to switch to the second camera it fails. It’s not just an issue with simultaneous camera but even switching to another camera produces an error.