Running the program under zed-sdk-5.0.7/depth sensing/multi camera/cpp, testing 4 cameras running; frame rate set to 60fps, mode selection is default; initially, the displayed frame rate is less than ~18 fps; after running for about a few dozen minutes, the terminal repeatedly prints an error message similar to: ERROR_CODE sl::grab(sl::RuntimeParameters). Observing the terminal output, the log information for one or more cameras stops being output, and the displayed frame rate for the remaining cameras increases significantly.
The module used is the Orin 64G module; Jetpack 6.2. Has set jetson_clocks.
What is the reason for this, and what are the directions for optimization?