Hi @Myzhar ,
The resolutions we are using are HD1200@60fps for all cameras and jetson power mode is set to MAXN. We have set jetson clocks are well.
The jetson cpu usage per core is around 85%, gpu usage is around 40% for the most part occasionally going upto 80% and falling back. The temperatures seem to be round about 55-60 degrees celcius.
Let me know if you need any other information. We have faced similar issue in the past where the streaming would seg fault after a while as we shared in this forum post.
But now the streaming does not raise a segmentation fault but the cameras reboot successfully after a while. Below, I am sharing the message from the forum post where we faced the same issue.
- We quite often observe the following error during streaming but the streaming again runs fine after a while and the jetson ram,cpu,gpu,temperature everything looks normal. One additional thing to note here is we have been monitoring the time interval between 2 consecutive frames and the error below comes when the time between 2 consecutive frames is ~10000ms. I have shared a link to all the logs at the bottom of this post
(Argus) Error Timeout: (propagating from src/rpc/socket/client/ClientSocketManager.cpp, function send(), line 137)
(Argus) Error Timeout: (propagating from src/rpc/socket/client/SocketClientDispatch.cpp, function dispatch(), line 92)
(Argus) Error InvalidState: Argus client is exiting with 11 outstanding client threads (in src/rpc/socket/client/ClientSocketManager.cpp, function recvThreadCore(), line 366)
(Argus) Error EndOfFile: Unexpected error in reading socket (in src/rpc/socket/client/ClientSocketManager.cpp, function recvThreadCore(), line 277)
(Argus) Error EndOfFile: Receive worker failure, notifying 11 waiting threads (in src/rpc/socket/client/ClientSocketManager.cpp, function recvThreadCore(), line 350)
(Argus) Error InvalidState: Argus client is exiting with 11 outstanding client threads (in src/rpc/socket/client/ClientSocketManager.cpp, function recvThreadCore(), line 366)
(Argus) Error EndOfFile: Receiving thread terminated with error (in src/rpc/socket/client/ClientSocketManager.cpp, function recvThreadWrapper(), line 379)
(Argus) Error InvalidState: Receive thread is not running cannot send. (in src/rpc/socket/client/ClientSocketManager.cpp, function send(), line 96)
(Argus) Error InvalidState: (propagating from src/rpc/socket/client/SocketClientDispatch.cpp, function dispatch(), line 92)
(Argus) Error InvalidState: Receive thread is not running cannot send. (in src/rpc/socket/client/ClientSocketManager.cpp, function send(), line 96)
(Argus) Error InvalidState: (propagating from src/rpc/socket/client/SocketClientDispatch.cpp, function dispatch(), line 92)
(Argus) Error InvalidState: Receive thread is not running cannot send. (in src/rpc/socket/client/ClientSocketManager.cpp, function send(), line 96)
(Argus) Error InvalidState: (propagating from src/rpc/socket/client/SocketClientDispatch.cpp, function dispatch(), line 92)