I’m running a ZED2i on a Jetson nano through ROS1 with a recent version of the ZED software as well as ROS. I get lots of
Elaboration takes longer (0.139038 sec) than the requested FPS rate (0.066666667 sec). Please consider to lower the 'frame_rate' setting or to reduce the power requirements reducing the resolutions
There is no “frame_rate” setting that I can see. There are quite a few rate and freq settings, but none have a value of 15. I have also inspected all the dynamic ones using the parameter server and none have a value of 15. Which am I supposed to change?
Thank you for confirming which parameter it is. Before answering your questions however, this parameter is set to 10 in my config file (confirmed by rosparam get). Why is it asking for 15?
I use VGA resolution, I have position tracking. I have experimented with mapping or not and that makes no difference.
jetson_clocks shows the power mode is MAXN. Current freqs are all at the max allowed. This is on a Jetson nano.
The message is related to the “grab time”. It says that your configuration is too hard for your hardware because it cannot reach the 15 FPS required for “grabbing”.