We are looking to use the following
1 ZED X Mini 2.2 mm GMSL2, and 2 Stereolabs ZED X One 4K Wide ZED-422010 GMSL2
I was wondering if there are drivers available for AVerMedia D331 + 61D317GM01AF + Thor T5000 platform that we are thinking of using.
We are looking to use the following
1 ZED X Mini 2.2 mm GMSL2, and 2 Stereolabs ZED X One 4K Wide ZED-422010 GMSL2
I was wondering if there are drivers available for AVerMedia D331 + 61D317GM01AF + Thor T5000 platform that we are thinking of using.
Hi @michael.sprauve,
welcome to the StereoLabs community, and thank you for your interest in our ZED X Mini and ZED X One 4K cameras.
I was wondering if there are drivers available for AVerMedia D331 + 61D317GM01AF + Thor T5000 platform that we are thinking of using.
The AVerMedia D331 is a third-party carrier board, so the ZED X Driver does not support it natively; the GMSL2 driver for this platform is provided and maintained by AVerMedia. You can find the StereoLabs camera driver package in the Download section of the AVerMedia GMSL Board page, and I recommend contacting AVerMedia Technical Support to confirm the correct package for your JetPack version and for your specific camera configuration.
Alternatively, you can sign a mutual NDA with StereoLabs to access the private ZED X Driver source repository and port it to your platform.
Best regards,
Myzhar