hello i am Using Docker zed3.8-cuda11.7-ubuntu20.04 ; i have build ros noetic on it and i tried building the zed_ros_wrapper package on the docker and i have been having the error in catkin_make
after passing catkin_make -DCUDA_TOOLKIT_ROOT_DIR=/usr/local/cuda i still have
CMake Error at /usr/share/cmake-3.16/Modules/FindPackageHandleStandardArgs.cmake:146 (message):
Could NOT find CUDA (missing: CUDA_NVCC_EXECUTABLE CUDA_INCLUDE_DIRS
CUDA_CUDART_LIBRARY) (Required is at least version “11”)
Call Stack (most recent call first):
/usr/share/cmake-3.16/Modules/FindPackageHandleStandardArgs.cmake:393 (_FPHSA_FAILURE_MESSAGE)
/usr/share/cmake-3.16/Modules/FindCUDA.cmake:1104 (find_package_handle_standard_args)
/usr/local/zed/zed-config.cmake:72 (find_package)
zed-ros-wrapper/zed_nodelets/CMakeLists.txt:22 (find_package)
– Configuring incomplete, errors occurred!
See also “/zed_ws/build/CMakeFiles/CMakeOutput.log”.
See also “/zed_ws/build/CMakeFiles/CMakeError.log”.
Invoking “cmake” failed
i tried passing the values for missing but still have the error.
please help me build this image or please guide me if there exist such docker image