Disabling IMU on GMSL ZED X / X One

Can the IMU be disabled on GMSL ZED X / X One if it is unused?

Hi @corentinartaud,
Welcome to the StereoLabs community.

No, the IMU of the ZED X and the ZED X One cannot be disabled; it is always powered and running at the hardware level, and its data stream is handled by the ZED X Driver and the ZED SDK with negligible overhead.

If you do not need inertial data, simply do not call getSensorsData, and set PositionalTrackingParameters::enable_imu_fusion to false if you use Positional Tracking without the IMU contribution.

More details about the sensors module are available in the online documentation.

Can you share the reason why you want to disable it? This will help me suggest the best configuration for your use case.

If the worry is CPU load or power draw, it may be worth measuring before assuming the IMU is the cause. As Myzhar says, it only produces data that nothing reads unless you call getSensorsData, so the cost should be small. If you also use positional tracking, turning off IMU fusion lets you compare tracking quality and CPU usage with and without it. A quick look at tegrastats or top with and without the sensors calls would show whether there is any real difference on your setup. If you can share what you are trying to save, such as latency, power or CPU, people here can probably suggest something more specific.