This happens on a fresh install of Ubuntu 24.04, with the default nvidia drivers. I immediately downloaded the ZED SDK 5.0 and run the Depth Viewer, and get the following stack trace, which appears to be a cuda crash. I did not explicitly install cuda.
[2025-05-08 14:37:19 UTC][ZED][INFO] [Init] Depth mode: NEURAL
[2025-05-08 14:37:20 UTC][ZED][INFO] [Init] Camera successfully opened.
[2025-05-08 14:37:20 UTC][ZED][INFO] [Init] Camera FW version: 1523
[2025-05-08 14:37:20 UTC][ZED][INFO] [Init] Video mode: HD720@30
[2025-05-08 14:37:20 UTC][ZED][INFO] [Init] Serial Number: S/N 35121213
[2025-05-08 14:37:20 UTC][ZED][INFO] [Init] No calibration file found for SN 35121213. Downloading...
[2025-05-08 14:37:20 UTC][ZED][INFO] [Init] Calibration file downloaded.
[2025-05-08 14:37:21 UTC][ZED][WARNING] [Init] Self-calibration skipped. Scene may be occluded or lack texture. (Error code: 0x01)
in bool ImageHandler::initialize(sl::Mat&) : Err [999]: unknown error.
Stack trace (most recent call last):
#24 Object "[0xffffffffffffffff]", at 0xffffffffffffffff, in
#23 Object "/usr/local/zed/tools/ZED_Depth_Viewer", at 0x59c0f7195c54, in
#22 Object "/lib/x86_64-linux-gnu/libc.so.6", at 0x79479ec2a28a, in __libc_start_main
#21 Object "/lib/x86_64-linux-gnu/libc.so.6", at 0x79479ec2a1c9, in
#20 Object "/usr/local/zed/tools/ZED_Depth_Viewer", at 0x59c0f7194dad, in
#19 Object "/lib/x86_64-linux-gnu/libQt5Core.so.5", at 0x79479f6df3e7, in QCoreApplication::exec()
#18 Object "/lib/x86_64-linux-gnu/libQt5Core.so.5", at 0x79479f6d6a7a, in QEventLoop::exec(QFlags<QEventLoop::ProcessEventsFlag>)
#17 Object "/lib/x86_64-linux-gnu/libQt5Core.so.5", at 0x79479f735278, in QEventDispatcherGlib::processEvents(QFlags<QEventLoop::ProcessEventsFlag>)
#16 Object "/lib/x86_64-linux-gnu/libglib-2.0.so.0", at 0x79479d913a52, in g_main_context_iteration
#15 Object "/lib/x86_64-linux-gnu/libglib-2.0.so.0", at 0x79479d973716, in
#14 Object "/lib/x86_64-linux-gnu/libglib-2.0.so.0", at 0x79479d9145b4, in
#13 Object "/lib/x86_64-linux-gnu/libQt5Core.so.5", at 0x79479f734f10, in
#12 Object "/lib/x86_64-linux-gnu/libQt5Core.so.5", at 0x79479f7345aa, in QTimerInfoList::activateTimers()
#11 Object "/lib/x86_64-linux-gnu/libQt5Core.so.5", at 0x79479f6d8117, in QCoreApplication::notifyInternal2(QObject*, QEvent*)
#10 Object "/lib/x86_64-linux-gnu/libQt5Widgets.so.5", at 0x7947a036bd44, in QApplicationPrivate::notify_helper(QObject*, QEvent*)
#9 Object "/lib/x86_64-linux-gnu/libQt5Core.so.5", at 0x79479f70624a, in QObject::event(QEvent*)
#8 Object "/lib/x86_64-linux-gnu/libQt5Core.so.5", at 0x79479f71710c, in QTimer::timeout(QTimer::QPrivateSignal)
#7 Object "/lib/x86_64-linux-gnu/libQt5Core.so.5", at 0x79479f712dbe, in
#6 Object "/usr/local/zed/tools/ZED_Depth_Viewer", at 0x59c0f71c8db1, in
#5 Object "/usr/local/zed/tools/ZED_Depth_Viewer", at 0x59c0f71c49da, in
#4 Object "/usr/local/zed/tools/ZED_Depth_Viewer", at 0x59c0f71d4829, in
#3 Object "/usr/local/zed/tools/ZED_Depth_Viewer", at 0x59c0f71d3308, in
#2 Object "/usr/local/zed/tools/ZED_Depth_Viewer", at 0x59c0f723c9ed, in
#1 Object "/usr/local/zed/tools/ZED_Depth_Viewer", at 0x59c0f71f46b2, in
#0 Object "/lib/x86_64-linux-gnu/libcuda.so.1", at 0x7947b2179218, in
Segmentation fault (Signal sent by the kernel [(nil)])
Segmentation fault (core dumped)
nvidia-smi reports:
$ nvidia-smi
Thu May 8 10:48:26 2025
+-----------------------------------------------------------------------------------------+
| NVIDIA-SMI 570.133.07 Driver Version: 570.133.07 CUDA Version: 12.8 |
|-----------------------------------------+------------------------+----------------------+
| GPU Name Persistence-M | Bus-Id Disp.A | Volatile Uncorr. ECC |
| Fan Temp Perf Pwr:Usage/Cap | Memory-Usage | GPU-Util Compute M. |
| | | MIG M. |
|=========================================+========================+======================|
| 0 NVIDIA GeForce RTX 4060 ... Off | 00000000:01:00.0 Off | N/A |
| N/A 40C P0 590W / 85W | 15MiB / 8188MiB | 14% Default |
| | | N/A |
+-----------------------------------------+------------------------+----------------------+
+-----------------------------------------------------------------------------------------+
| Processes: |
| GPU GI CI PID Type Process name GPU Memory |
| ID ID Usage |
|=========================================================================================|
| 0 N/A N/A 3377 G /usr/lib/xorg/Xorg 4MiB |
+-----------------------------------------------------------------------------------------+