Hi there,
I have compiled the spatial mapping example on Windows using this guide and would like to deploy the resulting .exe onto another Windows PC
My First PC has a NVIDIA RTX A2000 Laptop GPU, and GPU driver version (528.90) , with CUDA 11.8 toolkit installed.
I know CUDA 11.X is compatible with a minimum Nvidia Compute Capability of 3.5, but when compiling the spatial mapping example, I am unsure as to which GPU architectures the ZED application is compiling for…
- When compiling the ZED SDK samples, which architectures of NVidia GPUs are targeted? Is it currently to set to only compile for the currently discovered GPU?
- Am I able to compile for all GPU versions that are compatible with CUDA 11.X? e.g. Will the
execompiled on my laptop with anRTX A2000(compute capability 8.6) be able to be used with a PC with aGTX 1080(compute capability: 6) - If not, how can I target all compatible GPU versions (say, compute capability > 6.0) ?