Corrupted SDK Installation: Neural TRT not found

Recently an Error occurred, telling me my SDK installation is corrupted. However, the ZED_Depth_Viewer and ZED_Diagnostic Tools work fine nor show an error.

Only when running a Python Script and trying to open the camera it is reporting the error:

[2025-10-24 15:05:02 UTC][ZED][INFO] Logging level INFO
[2025-10-24 15:05:06 UTC][ZED][INFO] [Init]  Camera FW version: 2001
[2025-10-24 15:05:06 UTC][ZED][INFO] [Init]  Video mode: HD1080@30
[2025-10-24 15:05:06 UTC][ZED][INFO] [Init]  Serial Number: S/N 43874559
[2025-10-24 15:05:06 UTC][ZED][INFO] [Init]  Depth mode: NEURAL
[2025-10-24 15:05:06 UTC][ZED][ERROR] [Object Detection]  TensorRT library not found
[2025-10-24 15:05:06 UTC][ZED][ERROR] [ZED] [Depth]  NEURAL TRT NOT FOUND
[2025-10-24 15:05:06 UTC][ZED][ERROR] CORRUPTED SDK INSTALLATION in sl::ERROR_CODE sl::Camera::open(sl::InitParameters)
[2025-10-24 15:05:08 UTC][ZED][WARNING] [Init]  Self-calibration skipped. Scene may be occluded or lack texture.
Segmentation fault (core dumped)

I’m using a Jetson AGX Orin with the most recent GMSL2 DUO Driver (and card) with Jetpack 6.2 (R36.4.7), cuda 12.6, ZED SDK 5.1.0.
I already reinstalled the ZED SDK and deleted the /usr/local/zed folder. I reinstalled the GMSL Driver too.

I currently cant reflash my jetson, any help would be appreciated.

I solved it.

Importing ‘tensorrt’ in python failed and showed that ‘libcudla.so.1’ was missing.

Upgrading Jetpack helped to reinstall necessary packages:

sudo apt update
sudo apt dist-upgrade
sudo apt install --fix-broken -o Dpkg::Options::=“–force-overwrite”

It is now working again.