Corrupt SDK installation error when trıed to launch ros2 wrapper

we are having an issue with zed2i on our jetson agx orin we have ros2 installed correctly our nodes are working but when we try to run " ros2 launch zed_wrapper zed_camera.launch.py camera_model:=zed2i" code we have this error even though camera connected and some codes can be executed from vscode.
we use JP 6.1

HD720@30
[component_container_isolated-2] [2024-11-28 13:52:24 UTC][ZED][INFO] [Init]  Serial Number: S/N 39159302
[component_container_isolated-2] [2024-11-28 13:52:24 UTC][ZED][ERROR] [Object Detection]  TensorRT library not found
[component_container_isolated-2] [2024-11-28 13:52:24 UTC][ZED][ERROR] [ZED] [Depth]  NEURAL TRT NOT FOUND
[component_container_isolated-2] [2024-11-28 13:52:24 UTC][ZED][WARNING] CORRUPTED SDK INSTALLATION in sl::ERROR_CODE sl::Camera::open(sl::InitParameters)
[component_container_isolated-2] [2024-11-28 13:52:25 UTC][ZED][WARNING] [Init]  Self-calibration failed. Point the camera towards a more textured and brighter area. Avoid objects closer than 1 meter (Error code: 0x03) 
[component_container_isolated-2] [WARN] [1732801945.112425295] [zed.zed_node]: Error opening camera: CORRUPTED SDK INSTALLATION
[component_container_isolated-2] [INFO] [1732801945.112667022] [zed.zed_node]: Please verify the camera connection
[component_container_isolated-2] Movements detected during IMU initialization, please keep the camera steady
[component_container_isolated-2] [2024-11-28 13:52:30 UTC][ZED][INFO] Logging level INFO
[ERROR] [component_container_isolated-2]: process has died [pid 5906, exit code -11, cmd '/home/bylogix/ros2_humble/install/rclcpp_components/lib/rclcpp_components/component_container_isolated --ros-args -r __node:=zed_container -r __ns:=/zed'].
^C[WARNING] [launch]: user interrupted with ctrl-c (SIGINT)
[robot_state_publisher-1] [INFO] [1732801975.454970591] [rclcpp]: signal_handler(signum=2)
[INFO] [robot_state_publisher-1]: process has finished cleanly [pid 5904]

Hi @bartu
Welcome to the Stereolabs community.

Please try to use ZED_Explorer and ZED_Depth_Viewer and let me know if they work.

Please also launch ZED_Diagnostic and send me the report file that it generates.