I have hit a bit of a wierd issue with your newest SDK version. I use the following code to open a virtual stereo camera with two zed x one. The problem is that if i swap around the serial numbers, then i cant open the camera and i get error code “Camera failed to Setup”. The first time it happened i didnt bother looking into it, and just swapped around the cameras, but the issue is the correct order have now changed, so i would have to swap around and calibrate again. I can also replicate the issue with your virtual stereo example, so you can use that if you want to try to replicate.
unsigned int serial_left = 305743419;
unsigned int serial_right = 307994820;
unsigned int virt_sn = generateVirtualStereoSerialNumber(serial_left, serial_right);
init_parameters.input.setVirtualStereoFromSerialNumbers(serial_left, serial_right, virt_sn);