Cant detect cameras in ros2 wrapper

Would i by using them as monocular cameras be able to still synchronize them to the same accuracy, or is the synchronization handled by the media server?

I use the Orin NX 16, so that should support hardware encoding.

Do you have any other ideas of what i should investigate or change to use less resources on the media server? My requirements is basicly only to get synchronized image pairs and get the IMU data, so disabling the depth modules and other stuff would be okay if that could reduce the resources used

Synchronization happens at the hardware level. It’s SW independent

You must wait for a SW improvement on our side

Okay, how can i access them as monocular cameras? And would i still be able to get the IMU data?

In ROS 2 you must simply change camera_model in the launch command from virtual to zedxonegs

Yes, it’s published by the wrapper node.

When i launch the node with camera model zedxonegs it only opens one of the cameras, how do i open both as monocular cameras?

You must launch a node for each camera and distinguish them by camera_serial or camera_id.
Please read the multi-camera documentation here:

When i run this example or just run the ros2 wrapper on a single camera the node starts correctly, but once i subscribe to one of the topics the node crashes with the following error “[ERROR] [component_container_isolated-2]: process has died [pid 828547, exit code -11, cmd ‘/opt/ros/humble/lib/rclcpp_components/component_container_isolated --use_multi_threaded_executor --ros-args --log-level info --ros-args -r __node:=zed_container -r __ns:=/zed’].” It advertices the topics, but if i subscribe to any of them the node crashes

Please share your launch command

ros2 launch zed_wrapper zed_camera.launch.py camera_model:=zedxonegs. I can see it chooses the right serial number and it advertises the topics. I run it in docker with nvidia isaac ros container using your guide

We are working on a fix for this (ZED X One error). It will be available in the next few hours.

Sound good, thank you. If i just need to get images and imu data from the cameras without needing the rest of the SDK, should i then use the zedx-one-capture repo maybe? I want to simplify it as much as possible since all i need right now is synchronized video with imu data, but i cant see how to get the imu data from that repo. Can i use your regular SDK for these cameras without using the media server or is it only zedx-one-capture i can use for that?

The modification that we are applying is bigger, but you should be able to make it work by changing
pubImg.publish(std::move(image), std::move(camInfoMsg));
to
pubImg.publish(std::move(image), *camInfoMsg);

here:

This works correctly because the camera_info topic content does not change while the node runs

I added the changes you requested, but it cant compile since there is no matching function in image_transport it seems like. I get the following error:

/workspaces/isaac_ros-dev/src/zed-ros2-wrapper/zed_components/src/zed_camera/src/zed_camera_one_component.cpp: In member function ‘void stereolabs::ZedCameraOne::publishImageWithInfo(const sl::Mat&, const image_transport::CameraPublisher&, stereolabs::camInfoMsgPtr&, const string&, const rclcpp::Time&)’:
/workspaces/isaac_ros-dev/src/zed-ros2-wrapper/zed_components/src/zed_camera/src/zed_camera_one_component.cpp:2894:19: error: no matching function for call to ‘image_transport::CameraPublisher::publish(std::remove_reference<std::unique_ptr<sensor_msgs::msg::Image_<std::allocator<void> >, std::default_delete<sensor_msgs::msg::Image_<std::allocator<void> > > >&>::type, std::__shared_ptr_access<sensor_msgs::msg::CameraInfo_<std::allocator<void> >, __gnu_cxx::_S_atomic, false, false>::element_type&) const’
 2894 |     pubImg.publish(std::move(image), *camInfoMsg);
      |     ~~~~~~~~~~~~~~^~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~
In file included from /opt/ros/humble/include/image_transport/image_transport/image_transport.hpp:39,
                 from /workspaces/isaac_ros-dev/src/zed-ros2-wrapper/zed_components/src/tools/include/sl_types.hpp:32,
                 from /workspaces/isaac_ros-dev/src/zed-ros2-wrapper/zed_components/src/zed_camera/include/zed_camera_one_component.hpp:26,
                 from /workspaces/isaac_ros-dev/src/zed-ros2-wrapper/zed_components/src/zed_camera/src/zed_camera_one_component.cpp:15:
/opt/ros/humble/include/image_transport/image_transport/camera_publisher.hpp:103:8: note: candidate: ‘void image_transport::CameraPublisher::publish(const Image&, const CameraInfo&) const’
  103 |   void publish(
      |        ^~~~~~~
/opt/ros/humble/include/image_transport/image_transport/camera_publisher.hpp:104:37: note:   no known conversion for argument 1 from ‘std::remove_reference<std::unique_ptr<sensor_msgs::msg::Image_<std::allocator<void> >, std::default_delete<sensor_msgs::msg::Image_<std::allocator<void> > > >&>::type’ {aka ‘std::unique_ptr<sensor_msgs::msg::Image_<std::allocator<void> >, std::default_delete<sensor_msgs::msg::Image_<std::allocator<void> > > >’} to ‘const Image&’ {aka ‘const sensor_msgs::msg::Image_<std::allocator<void> >&’}
  104 |     const sensor_msgs::msg::Image & image,
      |     ~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~^~~~~
/opt/ros/humble/include/image_transport/image_transport/camera_publisher.hpp:111:8: note: candidate: ‘void image_transport::CameraPublisher::publish(const ConstSharedPtr&, const ConstSharedPtr&) const’
  111 |   void publish(
      |        ^~~~~~~
/opt/ros/humble/include/image_transport/image_transport/camera_publisher.hpp:113:58: note:   no known conversion for argument 2 from ‘std::__shared_ptr_access<sensor_msgs::msg::CameraInfo_<std::allocator<void> >, __gnu_cxx::_S_atomic, false, false>::element_type’ {aka ‘sensor_msgs::msg::CameraInfo_<std::allocator<void> >’} to ‘const ConstSharedPtr&’ {aka ‘const std::shared_ptr<const sensor_msgs::msg::CameraInfo_<std::allocator<void> > >&’}
  113 |     const sensor_msgs::msg::CameraInfo::ConstSharedPtr & info) const;
      |     ~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~^~~~
/opt/ros/humble/include/image_transport/image_transport/camera_publisher.hpp:123:8: note: candidate: ‘void image_transport::CameraPublisher::publish(sensor_msgs::msg::Image&, sensor_msgs::msg::CameraInfo&, rclcpp::Time) const’
  123 |   void publish(
      |        ^~~~~~~
/opt/ros/humble/include/image_transport/image_transport/camera_publisher.hpp:123:8: note:   candidate expects 3 arguments, 2 provided

Can i somehow just use the zedx-one-capture repo or similar to just get synced images and imu data from the cameras without the overhead of the ros wrapper and depth modules etc?

Sorry, it was a typo. This is the correct code:
pubImg.publish(std::move(image), camInfoMsg);

In any case, the fix is already applied to the master branch

Thank you, i will try that. Im also looking at just using your SDK for retrieving images and imu data without the ros wrapper. I see there is a tutorial for ZED X one for a single camera. If i use that and create a instance of the class CameraOne for each camera, would it then be synced or do i have to do something else to sync them when using your SDK? The example i am looking at is the file called live.cpp

Can you tell me how i with the SDK can get synced images and imu data from two zed x one gs? I am experiencing a lot of frame drops on the ros wrapper where there can be several frame periods between images from the cameras sometimes, which is a bit of a challenge for the vslam application i am using it for. I am using your zed multi example, and i already did the network tuning without luck, so all i would like is just how to get it from the SDK without ros wrapper and without zed media server.

If they are connected to the same GMSL2 port, they are natively hardware synchronized.

Do you know what could be the issue since the ros wrapper is dropping frames? It some times is up to 3 frames in a row. The published frame rate to the topics is around 26-27 fps even though it is set to 30, and the system isnt overloaded

Normally, it’s a simple power resource issue:

  • resolution too high
  • grab rate too high
  • power mode not correct (MAXN is required to maximize the performance)
  • jetson_clocks not running
  • Jetson not properly cooled
  • …

What Jetson model are you using? I do not remember if you already provided this information.