Hi I have zed 2i camera and I tried to install the supporting tools in jetsen xavier board with Ubuntu 20.04.6 LTS OS with disk space 16GB, while I install tools SDK and proceed before fully installation gets completed storage issue occurs and couldn’t proceed suggest the proper tools and solution for this issue.
Hi @User1
Welcome to the StereoLabs community.
Please post the full install log to check the error messages
Hi @User1
I recommend you read carefully the documentation of your Jetson device because I saw a lot of confusion:
- The NVIDIA SDK Manager is a tool to flash the Jetson device and install the NVIDIA library that must be installed on a host Ubuntu PC, not on the Jetson
- You must not install CUDA by using
apt, but by nstalling thejetpackpackage:sudo apt install nvidia-jetpack - Please do not show logs as screenshots, but copy the full log message and paste it into a txt file for easier access
Sorry for the confusion. I will share the full text log soon. This is my understanding.
- I can download SDK manager into a Ubuntu PC and flash the Jetson board with complete package.
(or) - I have existing Jetson board with Jetpack installed. I am trying to install Zedi specific package alone to test the camera.
- Pls point out the documentation for both #1 and #2
- I have Jetson Xavier platform which I am using for other purpose. I am worried about flashing it entirely with new image.
Applogies for inconvenience sir created
I couldn't attach the error text file due to new user, so I paste the complete log in as a post here.
**Low storage warning error:**
edge@ubuntu:-/Downloads
edge@ubuntu:-/Downloads$ sudo dpkg -1 sdkmanager 2.2.0-12021_amd64.deb [sudo] password for edge:
dpkg: error processing archive sdkmanager_2.2.0-12021_amd64.deb (--install):
package architecture (amd64) does not match system (arm64)
Errors were encountered while processing:
sdkmanager 2.2.0-12021_amd64.deb
edge@ubuntu:-/Downloads$ wget https://developer.download.nvidia.com/compute/cuda/repos/ubuntu2004/sbsa/cuda-ubuntu2004.pin
--2024-12-13 14:59:14-- https://developer.download.nvidia.com/compute/cuda/repos/ubuntu2004/sbsa/cuda-ubuntu2004.ptn Resolving developer.download.nvidia.com (developer.download.nvidia.com)... 152.199.39.144
Connecting to developer.download.nvidia.com (developer.download.nvidia.com) | 152.199.39.1441:443... connected.
HTTP request sent, awaiting response... 200 OK
Length: 190 [application/octet-stream]
Saving to: 'cuda-ubuntu2004.pin'
cuda-ubuntu2004.ptn 100% [======== ========>] 190 --.-KB/s in Os
2024-12-13 14:59:15 (1.28 MB/s) - 'cuda-ubuntu2004.pin' saved [190/190]
edge@ubuntu:-/Downloads$ sudo mv cuda-ubuntu2004.ptn /etc/apt/preferences.d/cuda-repository-pin-600
edge@ubuntu:~/Downloads
edge@ubuntu:-/Downloads$ wget https://developer.download.nvidia.com/compute/cuda/12.6.3/local_installers/cuda-repo-ubuntu2004-12-6-local_12.6.3-560.35.05-1_arm64.deb
--2024-12-13 14:59:35-- https://developer.download.nvidia.com/compute/cuda/12.6.3/local_installers/cuda-repo-ubuntu2004-12-6-local_12.6.3-560.35.05-1_arm64.deb Resolving developer.download.nvidia.com (developer.download.nvidia.com)... 152.199.39.144
Connecting to developer.download.nvidia.com (developer.download.nvidia.com) | 152.199.39.1441:443... connected.
HTTP request sent, awaiting response... 200 OK
Length: 2830539554 (2.6G) [application/x-deb]
Saving to: 'cuda-repo-ubuntu2004-12-6-local_12.6.3-560.35.05-1_arm64.deb'
cuda-repo-ubuntu200 100% [===================>] 2.64G 1.50MB/s in 11m 36s
2024-12-13 15:11:12 (3.88 MB/s) - 'cuda-repo-ubuntu2004-12-6-local_12.6.3-560.35.05-1_arm64.deb' saved [2830539554/2830539554]
edge@ubuntu:-/Downloads$ sudo dpkg -t cuda-repo-ubuntu2004-12-6-local_12.6.3-560.35.05-1_arm64.deb
Selecting previously unselected package cuda-repo-ubuntu2004-12-6-local.
(Reading database... 151698 files and directories currently installed.)
Preparing to unpack cuda-repo-ubuntu2004-12-6-local_12.6.3-560.35.05-1_arm64.deb...
Unpacking cuda-repo-ubuntu2004-12-6-local (12.6.3-560.35.05-1)
dpkg: error processing archive cuda-repo-ubuntu2004-12-6-local_12.6.3-560.35.05-1_arm64.deb (--install):
cannot copy extracted data for './var/cuda-repo-ubuntu2004-12-6-local/libcusparse-dev-12-6_12.5.4.2-1_arm64.deb' to '/var/cuda-repo-ubuntu2004-12-6-local/libcusparse-dev-12-6_12.5.4.2-1_arm64.deb.dpkg-n ew': failed to write (No space left on device) dpkg-deb: error: paste subprocess was killed by signal (Broken pipe)
Errors were encountered while processing:
cuda-repo-ubuntu2004-12-6-local_12.6.3-560.35.05-1_arm64.deb
edge@ubuntu:~/Downloads$ sudo dpkg -1 cuda-repo-ubuntu2004-12-6-local_12.6.3-560.35.05-1_arm64.deb
(Reading database... 151698 files and directories currently installed.)
Preparing to unpack cuda-repo-ubuntu2004-12-6-local_12.6.3-560.35.05-1_arm64.deb ...
Unpacking cuda-repo-ubuntu2004-12-6-local (12.6.3-560.35.05-1) ...
dpkg: error processing archive cuda-repo-ubuntu2004-12-6-local_12.6.3-560.35.05-1_arm64.deb (--install):
cannot copy extracted data for './var/cuda-repo-ubuntu2004-12-6-local/libnpp-12-6_12.3.1.54-1_arm64.deb' to '/var/cuda-repo-ubuntu2004-12-6-local/libnpp-12-6_12.3.1.54-1_arm64.deb.dpkg-new': failed to w rite (No space left on device) dpkg-deb: error: paste subprocess was killed by signal (Broken pipe)
Errors were encountered while processing:
cuda-repo-ubuntu2004-12-6-local_12.6.3-560.35.05-1_arm64.deb
edge@ubuntu:-/Downloads$
**Installation of CUDA error:**
edge@ubuntu:~/Downloads$ ll
total 83464
drwxr-xr-x 2 edge edge 4096 Dec 13 16:05 /
drwxr-xr-x 21 edge edge 4096 Dec 13 15:50 ../
--rw-rw-r-- 1 edge edge 920928 Dec 13 16:05 stereolabs-zedbox-onx16_1.2.1-LI-MAX96712-ALL-ZEDBOX-L4T35.4.1_arm64.deb
--rwxrwxr-x 1 edge edge 84529173 Dec 13 15.45 ZED_SDK_Tegra_L4T35.4_v4.2.2.zstd.run*
edge@ubuntu:~/Downloads$ chmod +x ZED_SDK_Tegra_L4T35.4_v4.2.2.zstd.run
edge@ubuntu:~/Downloads$ ./ZED_SDK_Tegra_L4T35.4_v4.2.2.zstd.run
Verifying archive integrity... 100% MD5 checksums are OK. All good.
Uncompressing 'ZED camera SDK by Stereolabs (Use 'sudo apt install zstd' if zstd is not found)' 100%
Detected Tegra_L4T35.5, required exact Tegra_L4T35.4
WARNING: possibly unsupported Linux 4 Tegra version, Continue [Y/n] ?n
Exiting
edge@ubuntu:~/Downloads$
Hi @User1
everything you are doing is wrong and the Jetson device is now in a bad status.
Please use the NVIDIA SDK Manager to reset it, but please read carefully the documentation of your Jetson device before beginning any other task.
Hi,
-
I read the documentation and followed the steps and done the reflashing of the Jetsen board.
-
Downloaded the SDk manager and installed it in a Ubuntu(20.04) pc and configured the steps for the Jetsen
-
While doing so facing issue at the time of Flashing the Jetsen linux the whole process completes and throws the error as below
“Installation failed”
I checked the log and here is the error message of the terminal below18:36:57.831 - Info: Waiting for device to expose ssh …Run command: flash on fc00:1:1:0::2
18:36:58.286 - Info: SSH ready
18:37:02.500 - Info: 4194304
18:37:02.531 - Info: [ 0]: l4t_flash_from_kernel: Serial Number: 1423323014629
18:37:02.532 - Info: [ 0]: l4t_flash_from_kernel: Starting to create gpt for emmc
18:37:02.533 - Info: Active index file is /mnt/internal/flash.idx
18:37:02.536 - Info: Number of lines is 42
18:37:02.536 - Info: max_index=41
18:37:06.372 - Info: [ 4]: l4t_flash_from_kernel: Successfully create gpt for emmc
18:37:06.373 - Info: [ 4]: l4t_flash_from_kernel: Starting to create gpt for external device
18:37:06.374 - Info: Active index file is /mnt/external/flash.idx
18:37:06.476 - Info: Number of lines is 18
18:37:06.476 - Info: max_index=17
18:37:06.664 - Info: writing item=1, 9:0:primary_gpt, 512, 19968, gpt_primary_9_0.bin, 16896, fixed--0, 4f10faef38eb9baef2f642279c90537fef54ae32
18:37:07.623 - Info: Error: Could not stat device /dev/nvme0n1 - No such file or directory.
18:37:07.646 - Info: Flash failure
18:37:07.646 - Info: Cleaning up…
18:37:08.780 - Error: [exec_command]: /bin/bash -c /home/user/.nvsdkm/replays/scripts/JetPack_5.1.4_Linux/NV_L4T_FLASH_JETSON_LINUX_COMP.sh; [error]: 87912 blocks
18:37:08.780 - Info: [ Component Install Finished with Error ]18:37:08.782 - Info: [host] [ 16.89 GB used. Disk Avail on Partition /dev/sda5: 537.36 GB ]18:37:08.782 - Info: [ NV_L4T_FLASH_JETSON_LINUX_COMP Install took 34m53s ]
@User1 This is an NVIDIA Jetson problem that requires support from the NVIDIA customer support team.
Please ask in the NVIDIA Developer Forum.