I am using a Jetson AGX Orin Dev Kit (64 Gb) with a dual stereo and four cameras connected.
ZED Explorer -a detects all cameras, but when trying to open the cameras with ZED_Depth Viewer or ZED_Explorer,it opens the first, but with the second it fails. I get:
[ZED][ERROR] [ZED] Cannot initialize the camera.
nvbuf_utils: dmabuf_fd -1 mapped entry NOT found
nvbuf_utils: dmabuf_fd -1 mapped entry NOT found
You are using 4 ZED X cameras connected to a ZED Link Duo capture card.
The problem could be caused by the fact that both ZED Explorer and ZED Depth Viewer are trying to open the cameras at 60 FPS in HD resolution, which is not supported for this configuration as explained here:
The error seems to persist when running the multi_camera example:
tmr-user@ubuntu:~/code/zed-sdk/depth sensing/multi camera/python$ python multi_camera.py Running… Opening ZED 55289125 [2025-10-17 15:23:51 UTC][ZED][INFO] Logging level INFO [2025-10-17 15:23:51 UTC][ZED][INFO] [Init] Depth mode: NEURAL [2025-10-17 15:23:55 UTC][ZED][INFO] [Init] Camera FW version: 2001 [2025-10-17 15:23:55 UTC][ZED][INFO] [Init] Video mode: HD1080@30 [2025-10-17 15:23:55 UTC][ZED][INFO] [Init] Serial Number: S/N 55289125 Optimized model not found, trying to download it… [2025-10-17 15:23:57 UTC][ZED][INFO] Please wait while the AI model is being optimized for your graphics card This operation will be run only once and may take a few minutes Optimizing neural_depth_5.3 | 100.0% [===================>] ETA: 0min 0s Opening ZED 47395504 [2025-10-17 15:28:43 UTC][ZED][INFO] Logging level INFO [2025-10-17 15:28:44 UTC][ZED][INFO] [Init] Depth mode: NEURAL [2025-10-17 15:29:06 UTC][ZED][ERROR] [ZED] Cannot initialize the camera. nvbuf_utils: dmabuf_fd -1 mapped entry NOT found nvbuf_utils: dmabuf_fd -1 mapped entry NOT found
Please try to run the command sudo service zed_x_daemon restart before trying to open the cameras again.
This will reset the ZED X Driver in case you plugged/unplugged cameras while the host was already booted. GMSL2 cameras are not plug-and-play; you cannot change the hardware configuration while the host is running.