I’m running 4 Zed Boxes all running the sample Camera Streamer code to a Fusion server. When I run the Camera Streamers from the terminal, we have great stability, and everything works great! However, today I moved them to a systemd service. The streamers run fantastically well and stay up, but the Fusion server (regardless of whether it’s run as a service or from the command line) rapidly (under 60 seconds) uses all of the system memory and is killed by the OOM OS manager. Is there a way I can run the streamer as a service, or maybe give it arguments that somehow reduce this memory usage?
For reference, when all the python scripts are run from the command line, the Fusion server holds steady at 5.7-5.8% of sytem memory for days at a time. When I run the streamers as a service, the Fusion server uses 100% of system memory within 60 seconds, and then crashes with a “Killed” message from the OS.
Just to clarify: we are using the Zed Boxes at a permanent installation, so we need them to be able to run as a service to handle reboots from power outages or maintenance automatically.
For anyone experiencing the same problem, it still currently exists, but we found a workaround by starting the scripts using gnome autostart in a terminal window, instead of using a systemd service.
Hello @pproctor,
Thank you for your feedback! To help us reproduce the issue, could you provide more details on how you are launching your sender with systemd? It would be helpful to know if you have checked that the clock used by the sender is synchronized when launched it with systemd.
Finally, to help us eliminate possible sources of error. Do you received fusion data before encountering the memory overflow issue or not ?
[Unit]
Description=Restarts sensorSender.py if it closes
[Service]
User=user
Type=simple
WorkingDirectory=/home/local/path/to
ExecStart=/usr/bin/python3 /home/local/path/to/sensorSender.py
Restart=always
[Install]
WantedBy=multi-user.target
Then we are adding the service using systemctl enable and systemctl start
The fusion script does receive data until it runs out of memory. Also, the sender scripts continue to run with no problem. Additionally, I am now running the fusion script as a service with no problems. The memory leak only occurs when the senders are running as services.
The sensorSender runs on 4 separate Zed Boxes, each with a single camera. To my knowledge there is no threading involved. It is the exact same code as your cameraSender sample, except that we change the port number using a CLI argument. Here’s the code:
import sys
import pyzed.sl as sl
import argparse
from time import sleep
def parse_args(init):
if ("HD2K" in opt.resolution):
init.camera_resolution = sl.RESOLUTION.HD2K
print("[Sample] Using Camera in resolution HD2K")
elif ("HD1200" in opt.resolution):
init.camera_resolution = sl.RESOLUTION.HD1200
print("[Sample] Using Camera in resolution HD1200")
elif ("HD1080" in opt.resolution):
init.camera_resolution = sl.RESOLUTION.HD1080
print("[Sample] Using Camera in resolution HD1080")
elif ("HD720" in opt.resolution):
init.camera_resolution = sl.RESOLUTION.HD720
print("[Sample] Using Camera in resolution HD720")
elif ("SVGA" in opt.resolution):
init.camera_resolution = sl.RESOLUTION.SVGA
print("[Sample] Using Camera in resolution SVGA")
elif ("VGA" in opt.resolution):
init.camera_resolution = sl.RESOLUTION.VGA
print("[Sample] Using Camera in resolution VGA")
elif len(opt.resolution)>0:
print("[Sample] No valid resolution entered. Using default")
else :
print("[Sample] Using default resolution")
def main():
init = sl.InitParameters()
init.camera_resolution = sl.RESOLUTION.AUTO
init.depth_mode = sl.DEPTH_MODE.NONE
init.sdk_verbose = True
parse_args(init)
output_port = opt.port
cam = sl.Camera()
status = cam.open(init)
if status != sl.ERROR_CODE.SUCCESS: #Ensure the camera has opened succesfully
print("Camera Open : "+repr(status)+". Exit program.")
exit()
runtime = sl.RuntimeParameters()
stream_params = sl.StreamingParameters()
stream_params.port = output_port
print("Streaming on port ",stream_params.port) #Get the port used to stream
stream_params.codec = sl.STREAMING_CODEC.H264
stream_params.bitrate = 4000
status_streaming = cam.enable_streaming(stream_params) #Enable streaming
if status_streaming != sl.ERROR_CODE.SUCCESS:
print("Streaming initialization error: ", status_streaming)
cam.close()
exit()
exit_app = False
try :
while not exit_app:
err = cam.grab(runtime)
if err == sl.ERROR_CODE.SUCCESS:
sleep(0.001)
except KeyboardInterrupt:
exit_app = True
# disable Streaming
cam.disable_streaming()
# close the Camera
cam.close()
if __name__ == "__main__":
parser = argparse.ArgumentParser()
parser.add_argument('--resolution', type=str, help='Resolution, can be either HD2K, HD1200, HD1080, HD720, SVGA or VGA', default = '')
parser.add_argument('--port', type=int, help='Port value for streaming', default = '30000')
opt = parser.parse_args()
main()`Preformatted text`
Keep in mind, there is no memory leak on this program. The memory leak comes from the Fusion server (also a separate machine) when it connects to these 4 streamers, if they are being run as a service.
My understanding is that the python implementation and the cpp implementation differ, and this is why the ClientPublisher sample doesn’t exist in python.
Could the Stereolabs team discuss and advise as to what the preferred implementation in python is?
The python and C++ implementation are the same. Only the sample is different. The C++ one use a proper thread for each ZED, the python one does every grab and process in the same thread because python threading is not reliable.
It’s not possible that your senders work without publishing the data. It’s also weird that your receiver would use startPublishing.
In the thread you mention, they are doing something quite specific: the sender are only streaming the raw RGB. Then, the receiver runs senders again, these open the streams and publish the data to the fusion. The prefered implementation would be that your receiver does not run all these publisher threads, that would be the job of the senders.
Now, that does not tell us why would the fusion module overflow the memory. Can you open all the streaming of your systemd services with ZED explorer ? What is the complete output of your receiver before it crashes ?
Just to be clear, despite what you’re saying, this is all working perfectly in both Zed Explorer and the Fusion server. The only time we see any problem is when the senders are run as services. Otherwise, everything works great.
The output receiver logs a connection for each Zed box it connects to, and then an OS kill message once it has used all the system memory. Again, this only happens when the senders are running as a systemd service.
Maybe you’re not understanding the implementation exactly; I used this sample as the basis for my fusion server: https://github.com/stereolabs/zed-sdk/blob/master/body%20tracking/multi-camera/python/fused_cameras.py You can see clearly on line 100 that it calls startPublishing on each of the cameraSenders after it connects. If this isn’t the preferred implementation, why is it in the only multi-camera sample?
I’d appreciate it if you could point me to a python sample that is the preferred implementation, if what we have done so far is not. As far as I can tell, there is no sample demonstrating the implementation you’re suggesting.
I did not say that it does not work, just that it is not very efficient. You have senders that create sl.Camera and streams only RGB, then a receiver that create sl.Camera again to compute the depth and, body tracking, etc., then the receiver also create a sl.Fusion object.
The recommended way would be to have your sender directly publish the data to the fusion, without the streaming, and the receiver only runs Fusion. The sample you are looking at is made for a USB workflow, where all the cameras are plugged to the same machine, this is why it does everything itself.
Unfortunately we don’t have a sample that demonstrates what I’m saying, but it is quite easy to build yourself. The sender is just like the tutorial 2, but it calls startPublishing. The receiver is just like the fusion sample you have, without the part where it starts cameras.
Wait, so for running Fusion over a local network to a Fusion server and Zed boxes connected to the cameras, all you need is startPublishing and subscribe? no start_streaming?
Would be wrong? You do not need to run the camera streaming sender example, you just need to open the camera and run startPublishing? So it would be something like this as the sender file?
init_params.input = conf.input_type
senders[conf.serial_number] = sl.Camera()
init_params.set_from_serial_number(conf.serial_number)
status = senders[conf.serial_number].open(init_params)
if status != sl.ERROR_CODE.SUCCESS:
print("Error opening the camera", conf.serial_number, status)
del senders[conf.serial_number]
continue
status = senders[conf.serial_number].enable_positional_tracking(positional_tracking_parameters)
if status != sl.ERROR_CODE.SUCCESS:
print("Error enabling the positional tracking of camera", conf.serial_number)
del senders[conf.serial_number]
continue
status = senders[conf.serial_number].enable_body_tracking(body_tracking_parameters)
if status != sl.ERROR_CODE.SUCCESS:
print("Error enabling the body tracking of camera", conf.serial_number)
del senders[conf.serial_number]
continue
senders[conf.serial_number].start_publishing(communication_parameters)
Should be a tutorial/example on this in zed-sdk/fusion as its not exactly clear besides this one comment:
Exactly. The comment you mention says that network camera are running there own code and publishing their data already. This sample only starts non-networked cameras.
Here is a sample that you can use for your sender:
import pyzed.sl as sl
def main():
# Create a Camera object
zed = sl.Camera()
# Create a InitParameters object and set configuration parameters
init_params = sl.InitParameters()
init_params.camera_resolution = sl.RESOLUTION.HD1080 # Use HD1080 video mode
init_params.camera_fps = 30 # Set fps at 30
# Open the camera
err = zed.open(init_params)
if err != sl.ERROR_CODE.SUCCESS:
print("Camera Open : "+repr(err)+". Exit program.")
exit()
ip = "192.168.1.50"
port = "300005"
communication_parameters = sl.CommunicationParameters()
communication_parameters.setForLocalNetwork(port, ip)
zed.start_publishing(communication_parameters)
# Capture 50 frames and stop
i = 0
image = sl.Mat()
runtime_parameters = sl.RuntimeParameters()
while True:
# Grab an image, a RuntimeParameters object must be given to grab()
if zed.grab(runtime_parameters) == sl.ERROR_CODE.SUCCESS:
# A new image is available if grab() returns SUCCESS
zed.retrieve_image(image, sl.VIEW.LEFT)
timestamp = zed.get_timestamp(sl.TIME_REFERENCE.CURRENT) # Get the timestamp at the time the image was captured
print("Image resolution: {0} x {1} || Image timestamp: {2}\n".format(image.get_width(), image.get_height(),
timestamp.get_milliseconds()))
i = i + 1
# Close the camera
zed.close()
if __name__ == "__main__":
main()
The solution from Benj was a workaround, not the recommended stuff.
I think you mistook someone else’s reply for mine, above. Unfortunately, I don’t have the ability to run tests on my hardware because it is installed on site in a running installation. I may be able to integrate the changes you mention at some future date.