I need some help to figure out the exact problem of camera connection issue so I can instruct a remote customer to replace the needed hardware. We frequently have customer facing similar problem and couldn’t figure out what could be wrong. We test the returned cameras from customer but they work fine.
We have the setup of 10m usb cable, zed box orin nx or xavier nx and zed2i, all ordered from stereolabs store.
The problem is the camera is not detected by the system, let alone the SDK, it’s not listed in /dev/video* at all. Here are some output that might be useful, please let me know if any other command is needed.
>> lsusb
Bus 002 Device 001: ID 1d6b:0003 Linux Foundation 3.0 root hub
Bus 001 Device 016: ID 2b03:f881 USB2.0 Hub
Bus 001 Device 015: ID 0424:2514 Microchip Technology, Inc. (formerly SMSC) USB 2.0 Hub
Bus 001 Device 005: ID 2109:2211 VIA Labs, Inc.
Bus 001 Device 003: ID 2109:2211 VIA Labs, Inc. USB2.0 Hub
Bus 001 Device 004: ID 148f:5370 Ralink Technology, Corp. RT5370 Wireless Adapter
Bus 001 Device 002: ID 05e3:0608 Genesys Logic, Inc. Hub
Bus 001 Device 001: ID 1d6b:0002 Linux Foundation 2.0 root hub
>> ls /dev/video*
ls: cannot access '/dev/video*': No such file or directory
Attached the dmesg output
dmesg.txt (76.5 KB)
Please instruct me what else is needed. Thanks