I am running a Jetson Orin AGX connected to a Stereolabs ZED Link Capture Card Quad. I have four ZedXOne GMSL cameras connected to this setup.
The problem is that the cameras are not being detected. Running the command ZED_Explorer -a lists no cameras. Crucially, the cameras are also not generating any heat, which strongly suggests a lack of power delivery.
Debugging Step: I measured the current draw and found that the capture card (with 4 dummy cameras connected) is only pulling 1.4 mA at 24V in its idle state. This is significantly low. I suspect a power issue with the card itself or the GMSL power distribution system.
Setup Context:
- System Status: This is a existing setup. It has previously worked correctly.
Could you please advise on what steps I should take to isolate this suspected power issue on the capture card?
Thank you, and looking forward to your fast support!