Build zed-gstreamer error

pls

nvidia@miivii-tegra:~$ cd zed-gstreamer/
nvidia@miivii-tegra:~/zed-gstreamer$ mkdir build
nvidia@miivii-tegra:~/zed-gstreamer$ cd build/
nvidia@miivii-tegra:~/zed-gstreamer/build$ cmake -DCMAKE_BUILD_TYPE=Release ..
-- The C compiler identification is GNU 9.4.0
-- The CXX compiler identification is GNU 9.4.0
-- Check for working C compiler: /usr/bin/cc
-- Check for working C compiler: /usr/bin/cc -- works
-- Detecting C compiler ABI info
-- Detecting C compiler ABI info - done
-- Detecting C compile features
-- Detecting C compile features - done
-- Check for working CXX compiler: /usr/bin/c++
-- Check for working CXX compiler: /usr/bin/c++ -- works
-- Detecting CXX compiler ABI info
-- Detecting CXX compiler ABI info - done
-- Detecting CXX compile features
-- Detecting CXX compile features - done
Running on NVIDIA Jetson
 * Found L4T v35.3.1
-- Found PkgConfig: /usr/bin/pkg-config (found version "0.29.1")
-- Checking for module 'gstreamer-1.0'
--   Found gstreamer-1.0, version 1.16.3
-- Checking for module 'gstreamer-base-1.0'
--   Found gstreamer-base-1.0, version 1.16.3
-- Found GSTREAMER_BASE_LIBRARY: /usr/lib/aarch64-linux-gnu/libgstbase-1.0.so
-- Found GSTREAMER_BASE_INCLUDE_DIR: /usr/include/gstreamer-1.0
-- Found GStreamer: /usr/lib/aarch64-linux-gnu/libgstreamer-1.0.so
-- Checking for module 'gstreamer-plugins-base-1.0'
--   Found gstreamer-plugins-base-1.0, version 1.16.3
-- Checking for module 'gstreamer-video-1.0'
--   Found gstreamer-video-1.0, version 1.16.3
-- Found GSTREAMER_VIDEO_LIBRARY: /usr/lib/aarch64-linux-gnu/libgstvideo-1.0.so
-- Found GSTREAMER_VIDEO_INCLUDE_DIR: /usr/include/gstreamer-1.0
-- Found GStreamerPluginsBase: TRUE
-- Checking for module 'glib-2.0'
--   Found glib-2.0, version 2.64.6
-- Found GLIB2: /usr/lib/aarch64-linux-gnu/libglib-2.0.so
-- Checking for module 'gobject-2.0'
--   Found gobject-2.0, version 2.64.6
-- Found GObject: /usr/include/glib-2.0
-- Looking for sgemm_
-- Looking for sgemm_ - not found
-- Looking for pthread.h
-- Looking for pthread.h - found
-- Performing Test CMAKE_HAVE_LIBC_PTHREAD
-- Performing Test CMAKE_HAVE_LIBC_PTHREAD - Failed
-- Looking for pthread_create in pthreads
-- Looking for pthread_create in pthreads - not found
-- Looking for pthread_create in pthread
-- Looking for pthread_create in pthread - found
-- Found Threads: TRUE
-- Looking for sgemm_
-- Looking for sgemm_ - found
-- Found BLAS: /usr/lib/aarch64-linux-gnu/libopenblas.so
-- Found CUDA: /usr/local/cuda-11.4 (found suitable version "11.4", minimum required is "11.4")
-- Found CUDA: /usr/local/cuda-11.4 (found suitable exact version "11.4")
-- Found OpenCV: /usr (found version "4.5.4")
-- Checking for module 'gstreamer-rtsp-server-1.0>=1.14.5'
--   Found gstreamer-rtsp-server-1.0, version 1.16.2

Plugin install dir:
/usr/lib/aarch64-linux-gnu/gstreamer-1.0

Library install dir:
/usr/lib/aarch64-linux-gnu

Include install dir:
/usr/include/gstreamer-1.0/gst/zed

Executable install dir:
/usr/bin

 * gstzedmeta library added
   gstzedmeta: OS Unix
   gstzedmeta: Release mode
 * gstzedsrc plugin added
   gstzedsrc: OS Unix
   gstzedsrc: Release mode
 * gstzedxonesrc plugin added
   gstzedxonesrc: OS Unix - L4T
   gstzedxonesrc: Release mode
 * gstzeddemux plugin added
   gstzeddemux: OS Unix
   gstzeddemux: Release mode
 * gstzeddatamux plugin added
   gstzeddatamux: OS Unix
   gstzeddatamux: Release mode
 * gstzeddatacsvsink plugin added
   gstzeddatacsvsink: OS Unix
   gstzeddatacsvsink: Release mode
 * gstzedodoverlay plugin added
   gstzedodoverlay: OS Unix
   gstzedodoverlay: Release mode
 * gst-zed-rtsp-launch RTSP server application
   gst-zed-rtsp-launch: OS Unix
   gst-zed-rtsp-launch: Release mode

-----------------------------------------------------------------------------
-- The following external packages were located on your system.
-- This installation will have the extra features provided by these packages.
-----------------------------------------------------------------------------
   * GStreamer - Required to build
   * GStreamer base library - Required to build
   * GStreamer video library - Required to build
   * GLib - Required to build
   * GObject - Required to build
   * ZED SDK - Required to build 'gstzed'
   * Nvidia CUDA library - Required to build 'gstzed'
   * OpenCV library - Required to build 'gstzedodoverlay'
   * GSTREAMER RTSP SERVER library - Required to build 'gstrtspserver'

-----------------------------------------------------------------------------
-- Congratulations! All external packages have been found.
-----------------------------------------------------------------------------

-- Configuring done
-- Generating done
-- Build files have been written to: /home/nvidia/zed-gstreamer/build
nvidia@miivii-tegra:~/zed-gstreamer/build$ make
Scanning dependencies of target gstzedmeta
[  6%] Building CXX object gst-zed-meta/CMakeFiles/gstzedmeta.dir/gstzedmeta.cpp.o
[ 12%] Linking CXX shared library libgstzedmeta.so
[ 12%] Built target gstzedmeta
Scanning dependencies of target gstzedsrc
[ 18%] Building CXX object gst-zed-src/CMakeFiles/gstzedsrc.dir/gstzedsrc.cpp.o
[ 25%] Linking CXX shared module libgstzedsrc.so
[ 25%] Built target gstzedsrc
Scanning dependencies of target gstzedxonesrc
[ 31%] Building CXX object gst-zedxone-src/CMakeFiles/gstzedxonesrc.dir/gstzedxonesrc.cpp.o
In file included from /home/nvidia/zed-gstreamer/gst-zedxone-src/gstzedxonesrc.cpp:29:
/home/nvidia/zed-gstreamer/gst-zedxone-src/gstzedxonesrc.h:27:10: fatal error: sl/CameraOne.hpp: 没有那个文件或目录
   27 | #include "sl/CameraOne.hpp"
      |          ^~~~~~~~~~~~~~~~~~
compilation terminated.
make[2]: *** [gst-zedxone-src/CMakeFiles/gstzedxonesrc.dir/build.make:63:gst-zedxone-src/CMakeFiles/gstzedxonesrc.dir/gstzedxonesrc.cpp.o] 错误 1
make[1]: *** [CMakeFiles/Makefile2:351:gst-zedxone-src/CMakeFiles/gstzedxonesrc.dir/all] 错误 2
make: *** [Makefile:130:all] 错误 2

Hi @gitPff
are you using the latest ZED SDK v4.2.2?

Yes, I later updated the SDK, but when I used v4.2.2, the camera couldn’t play, so I created a new posthttps://community.stereolabs.com/t/after-updating-the-sdk-to-v4-2-2-the-camera-cannot-play/7698/2?u=gitpff

If I use ZED_SDK_Tegra_L4T35.3v4.1.4.zstd.run, I will not be able to compile through zed-gsstreamer
If I use ZED_SDK_Tegra_L4T35.3-v4.2.2.zstd.run, I won’t be able to play the camera
My driver version is v1.0.5