Hi,
I am trying to run the body tacking c# sample , with Zed SDK 4.0.3 and CUDA 12.1 on my machine.
This sample stops at optimizing the skeletal structure
Optimizing skeleton_body38_3.5 \ 0.3%[> ] 33min 14s est. left Could not locate **cublasLt64_11.dll.** Please make sure it is in your library path!
For Python Sample as well the same issue occured
I checked the CUDA toolkit and it has reference to cublasLt64_12.dll
Can you advise what needs to be done to use the installed cublasLT64 version
Thanks
Rahul