Body 18 vs. Body 34/38 (body tracking)

For body-tracking, does body18 have a further tracking range compared to body34/38?

I’m body-tracking using a pair of ZedXOneGS Wide-lensed cameras on body 34 (resulting in a range of ~5-6m in my application).

Does the reduced number of keypoints in body18 make any difference in terms of the tracking range?

Hi @dsalasidis
In your case, the Body Tracking range is not limited by a software configuration (the used model does not influence the depth range), but depends on the baseline that you set for your custom depth camera.
The wider the baseline, the longer the skeleton detection range.

Stereolabs Image: Setting up your Stereo Rig with two ZED X One cameras – Help Center | Stereolabs

I have a 34.5cm baseline between my cameras, which results in that ~5-6m depth range when body tracking with body34.

According to this image, the 34.5cm baseline should result in a depth range of ~100m.

I was wondering why my 34.5cm baseline is only providing body tracking at a depth range of up to ~5-6m (with body34)?

Is the stereo calibration accurate? Can you record a Stereo SVO with your system and share it with me together with the calibration file?

I sent you a private message including the Stereo SVO and the calibration file.

Let me know if you got it.

Please send a link here, or send an email to support@stereolabs.com with a link to this thread if the video cannot be publicly shared.

Hi @dsalasidis
I tested your SVO with the default setup of the C++ Body Tracking sample, and I found no issues.
The skeleton is detected and tracked in all the frames.

Have you copied the calibration file to the settings folder of the ZED SDK?