Assistance Required for Managing Multiple Camera Streams

Hi,

I’m encountering an issue while trying to receive streams from multiple cameras and serve them on a web interface using Flask.

My objectives are:

Ensure that the streaming runs smoothly and continuously without any interruptions.
Guarantee that if one camera fails, it does not affect the streaming of the other cameras.
My current approach involves receiving the streams and serving them via Flask on the same laptop, which can be accessed by anyone on the same network.

Here’s what I’ve tried so far:

Multiprocessing: This method handles failures gracefully, but I experience a brief glitch (like a blink) in all camera streams every 10 seconds.
Sequential code or threading: This method provides perfect streaming, but if one camera fails, all streams stop for approximately 15 seconds before resuming, This occurs regardless of whether there are 2 or more cameras.

Could you please advise on how to resolve these issues? I’m looking for a solution within the existing approach, as I do not have the time to explore entirely different methods.

Thank you for your assistance.

@Myzhar
@mattrouss
Please assist :pray:

Hi @ashfaq
we do not provide official plugins for Flask, so we cannot provide you with the correct reply to solve your problem.

In my opinion, when using multiple cameras, a multi-threading approach is the correct solution to make the system stable and fail-proof, but you must be sure that everything is correctly synchronized.
A wrong synchronization mechanism probably causes the glitch that you are facing every 10 seconds.

Thank u Mr. Myzhar for ur response

Can I send the code for u and assist me in it, please ?

My concern with threading is :

“without flask” if single cam is failed all cam is stopped. And resumed after 15 seconds

This isn’t acceptable, because i want both smoothly streaming without glitching and avoid single failure.

I’m sorry, but this is out of the scope of this support because it’s too specific to your configuration.

This should not happen if each camera runs in its own thread.

ashfaq:

Can I send the code for u and assist me in it, please ?

I’m sorry, but this is out of the scope of this support because it’s too specific to your configuration.

ashfaq:

My concern with threading is :

“without flask” if single cam is failed all cam is stopped. And resumed after 15 seconds

This should not happen if each camera runs in its own thread.

[Discourse post]

Walter

Walter Lucetti
Senior Computer Engineer
SDK / Robotics / HW
Stereolabs Support

I understand u Mr

I tried the multi camera code which is on ur website and once disconnect one cam. Both is stopped and second one is resumed again only frame in each 5 s3conds mainly ???

This means the single failure isnt handled 100% on ur samples, can assist only on ur code u provided on the website ?

########################################################################
#
# Copyright (c) 2020, STEREOLABS.
#
# All rights reserved.
#
# THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS
# "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT
# LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
# A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT
# OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL,
# SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT
# LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,
# DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY
# THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT
# (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE
# OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
#
########################################################################

"""
    Multi cameras sample showing how to open multiple ZED in one program
"""

import pyzed.sl as sl
import cv2
import numpy as np
import threading
import time
import signal

zed_list = []
left_list = []
depth_list = []
timestamp_list = []
thread_list = []
stop_signal = False

def signal_handler(signal, frame):
    global stop_signal
    stop_signal=True
    time.sleep(0.5)
    exit()

def grab_run(index):
    global stop_signal
    global zed_list
    global timestamp_list
    global left_list
    global depth_list

    runtime = sl.RuntimeParameters()
    while not stop_signal:
        err = zed_list[index].grab(runtime)
        if err == sl.ERROR_CODE.SUCCESS:
            zed_list[index].retrieve_image(left_list[index], sl.VIEW.LEFT)
            zed_list[index].retrieve_measure(depth_list[index], sl.MEASURE.DEPTH)
            timestamp_list[index] = zed_list[index].get_timestamp(sl.TIME_REFERENCE.CURRENT).data_ns
        time.sleep(0.001) #1ms
    zed_list[index].close()
	
def main():
    global stop_signal
    global zed_list
    global left_list
    global depth_list
    global timestamp_list
    global thread_list
    signal.signal(signal.SIGINT, signal_handler)

    print("Running...")
    init = sl.InitParameters()
    init.camera_resolution = sl.RESOLUTION.HD720
    init.camera_fps = 30  # The framerate is lowered to avoid any USB3 bandwidth issues

    #List and open cameras
    name_list = []
    last_ts_list = []
    cameras = sl.Camera.get_device_list()
    index = 0
    for cam in cameras:
        init.set_from_serial_number(cam.serial_number)
        name_list.append("ZED {}".format(cam.serial_number))
        print("Opening {}".format(name_list[index]))
        zed_list.append(sl.Camera())
        left_list.append(sl.Mat())
        depth_list.append(sl.Mat())
        timestamp_list.append(0)
        last_ts_list.append(0)
        status = zed_list[index].open(init)
        if status != sl.ERROR_CODE.SUCCESS:
            print(repr(status))
            zed_list[index].close()
        index = index +1

    #Start camera threads
    for index in range(0, len(zed_list)):
        if zed_list[index].is_opened():
            thread_list.append(threading.Thread(target=grab_run, args=(index,)))
            thread_list[index].start()
    
    #Display camera images
    key = ''
    while key != 113:  # for 'q' key
        for index in range(0, len(zed_list)):
            if zed_list[index].is_opened():
                if (timestamp_list[index] > last_ts_list[index]):
                    cv2.imshow(name_list[index], left_list[index].get_data())
                    x = round(depth_list[index].get_width() / 2)
                    y = round(depth_list[index].get_height() / 2)
                    err, depth_value = depth_list[index].get_value(x, y)
                    if np.isfinite(depth_value):
                        print("{} depth at center: {}MM".format(name_list[index], round(depth_value)))
                    last_ts_list[index] = timestamp_list[index]
        key = cv2.waitKey(10)
    cv2.destroyAllWindows()

    #Stop the threads
    stop_signal = True
    for index in range(0, len(thread_list)):
        thread_list[index].join()

    print("\nFINISH")

if __name__ == "__main__":
    main()

@Myzhar
Kindly assist

Hi @ashfaq,

What are the cameras that you are using? Are you using ZED 2 USB cameras or ZED X GMSL?

@mattrouss
Zed2i USB cameras

Hi @ashfaq,

Our code examples shared on our Github are code samples. They are meant to be used to get started with using the ZED SDK, and are by no means designed or meant for production applications.

There are many comments I can make about this sample regarding it not being a production-ready application, but generally speaking:

  • error codes must be checked. Here only the successful error code of the camera is handled, the application should behave different if the camera returns an error
  • the application uses python multi-threading, which is technically not multi-threading because of the GIL: What Is the Python Global Interpreter Lock (GIL)? – Real Python

What I would recommend is to either write the sample in C++, which provides really multi-threading, or make the sample sequential as you’ve stated before, and handle the errors from the ZED SDK on a failure.

I believe the cameras hang for 15s after a camera is disconnected, because the grab() call is blocking after a failure, as it runs its automatic recovery process. You can change this by setting this parameter to True: async_grab_camera_recovery