Device: jetson orin nano
Camera: zed2i
Camera FW version: 1523
SDK Version: 4.2.5
nvidia-jetpack 6.1
nvidia-l4t-core 36.4.3
cuda 12.6
Greetings,
I updated my jetson orin nano to 6.1 and the zed sdk to 4.2.5 I get the following error after I close the program. I did not have this before the update. I am using the c library sdk and have compiled and ran most current version on the github. This error was produced after compiling and running the c version of tutorial 1. The program seems to run fine. Is this an issue with Nvidia? I am using SSH to connect to the jetson. Thank you for any direction.
(Argus) Error EndOfFile: Unexpected error in reading socket (in src/rpc/socket/client/ClientSocketManager.cpp, function recvThreadCore(), line 277)
(Argus) Error EndOfFile: Receive worker failure, notifying 1 waiting threads (in src/rpc/socket/client/ClientSocketManager.cpp, function recvThreadCore(), line 350)
(Argus) Error InvalidState: Argus client is exiting with 1 outstanding client threads (in src/rpc/socket/client/ClientSocketManager.cpp, function recvThreadCore(), line 366)
(Argus) Error EndOfFile: Receiving thread terminated with error (in src/rpc/socket/client/ClientSocketManager.cpp, function recvThreadWrapper(), line 379)
(Argus) Error EndOfFile: Client thread received an error from socket (in src/rpc/socket/client/ClientSocketManager.cpp, function send(), line 145)
(Argus) Error EndOfFile: (propagating from src/rpc/socket/client/SocketClientDispatch.cpp, function dispatch(), line 92)
hey @Myzhar ,
I get the same issue nvbuf_utils: dmabuf_fd -1 mapped entry NOT found nvbuf_utils: dmabuf_fd -1 mapped entry NOT found (Argus) Error Timeout: (propagating from src/rpc/socket/client/ClientSocketManager.cpp, function send(), line 137) (Argus) Error Timeout: (propagating from src/rpc/socket/client/SocketClientDispatch.cpp, function dispatch(), line 91) (Argus) Error FileOperationFailed: Failed socket read: Connection reset by peer (in src/rpc/socket/common/SocketUtils.cpp, function readSocket(), line 79) (Argus) Error FileOperationFailed: Unexpected error in reading socket (in src/rpc/socket/client/ClientSocketManager.cpp, function recvThreadCore(), line 277) (Argus) Error FileOperationFailed: Receive worker failure, notifying 2 waiting threads (in src/rpc/socket/client/ClientSocketManager.cpp, function recvThreadCore(), line 350) (Argus) Error InvalidState: Argus client is exiting with 2 outstanding client threads (in src/rpc/socket/client/ClientSocketManager.cpp, function recvThreadCore(), line 366) (Argus) Error FileOperationFailed: Receiving thread terminated with error (in src/rpc/socket/client/ClientSocketManager.cpp, function recvThreadWrapper(), line 379) (Argus) Error FileOperationFailed: Client thread received an error from socket (in src/rpc/socket/client/ClientSocketManager.cpp, function send(), line 145) (Argus) Error FileOperationFailed: (propagating from src/rpc/socket/client/SocketClientDispatch.cpp, function dispatch(), line 91)
but even my camera is not initialized for some reason? and even with ZED_Explorer the gui shows the waiting for camera, and in the terminal it prints no valid camera. The ZED_Explorer --all detects the zedx camera correctly what is the issue?