Dear ZED Community,
i’ve gone thru hell the past days trying to get my jetson nano and zed2 up and running. I bought some years ago when i had some spare time a Jetson Nano B01 and a ZED2, cause i wanted to get into ai racing, ros in general, also had the idea of building my own lawnmower… but ye i endet up in a big project then some family stuffed happened and now i find myself some years down the road with the old hardware and again some time to spare… and i thought… why not give it a shot.
After checking tons of versions and compatibility stuff i tried my best and after figuring out that the flashing of the jetson is not just downloading an image anymore, its more of connecting as mutch cables as you possibly can attach to it i finally have Jetson SDK 4.6.4 running and tryed again the zedsdk, but it keeps failing on something the internet seems to be somewhat full of tips but then again i think they misleading as i am on a jetson that should have numpy and all that preconfigured…
Anyway back to my point, where i would be more then thankful for some advice from people that are deeper into this than i am at the moment.
So i have this some years old Jetson Nano. I have some pi cam’s that are compatible, also some webcams and the zed2. I did figure out that the zed2 is anyway to powerful to work with the Nano cause of the RAM constraints. Found that somewhere here in the Forum. I also have a pretty beefy home pc with some gaming cards in it. And i have fair amount of knowledge when it comes to C/C++/Python and Go.
So what would be your advice if i wanna end up somewhere down the road with a little robot that naviagtes thru my flat. Should i throw the Nano and get an Orin and do there the basic opencv tutorials there, cause it seems this is where it all starts.
Or should i use my home pc and some basic camera to get into it and then start working with the Zed2 to get comfortable.
However as a veteran in coding just getting into image processing/ml and that stuff i know its a pretty big field, but what would be your advice if you read this and know that i am atm not want to do my own models but using some later down the road after getting comfortable with all the library’s.
ty for your help
dom