Hello Stereolabs Team,
I am writing to you in order to obtain advice and clarifications regarding best practices for multiple issues.
Context: We have 5+ ZED Box Orin NX 16gb (with ZED X cameras); 2 of them had just returned from warranty and the state appears as new (we didn’t note the old serials in order to compare them but this is probably not relevant); The image and version they come with is different from the latest flash image found in your docs: 36.4.4 vs 36.4.3;
I want to know if it’s a good idea to make a flash backup of the factory image since it is 36.4.4 and the L4T have correct priorities set and it’s upgrade safe, but I’ve also encountered the following issues and have specific questions as well:
-
NEW ZED Boxes (36.4.4): ZED_Diagnostic reports that I have both SDK and GMSL driver installed but there’s no camera being detected, even after zed_x_daemon and nvargus restart + reboot (even tried all 4 camera cable splits); (No SDK / driver reinstall was done so far - wanted to clarify first what’s the actual issue, if any); The attached ZED_Diagnostic data is from here.
-
Why does the official post flash procedure recommend apt upgrade (without any hold or priority set) when from my experience this breaks the system by upgrading to 36.4.7 - which is not supported! What’s the correct procedure to have a stable system and installation starting from a flash?
-
See attached screenshot - it just happened after a reboot command on a new ZED Box - so far I’ve only installed epiphany-browser and anydesk!
-
After flashing a ZED Box (with JetPack 6.2 and 36.4), I’m unable to use the WIFI and fixing it took long enough that I gave up trying and just used the wireless from my attached MikroTik - but the factory 36.4.4 image comes with a working WIFI. (I tried the usual recommended WIFI fixes after flashing but without success)
-
One of the ZED Boxes (same version as others) has a non working reboot! Each reboot = shutdown; it’s not a first generation ZED Box - it doesn’t get fixed by flashing and the issue did not replicate on other ZED Boxes - any idea what’s the issue and how to fix it? (I even tried to flash the QSPI but the reboot was not fixed)
Thank you for your attention and we hope to solve and clarify all of the above!
All the best!
- I was not allowed to upload - as I’m considered to be a new user!
Here are the diagnostic JSON files and the image with the shutdown error
Download a1c94056-d87e-4cea-bc10-cfae11c0b28d.jpg | LimeWire