I’m using the ZED 2i with the official StereoLabs USB C to A 5m cable, and it’s connected through two USB 3.0 panel type connectors.
I’m using USB 3.1 repeaters at each stage, but between the panels, I’m using a USB A to A Male cable. However, this part currently doesn’t have a repeater, and the length is about 1.8 meters.
Do you have any experience with using a USB A to A male active cable or something similar?
If the panel type USB connectors are short (around 1 meter or less), they don’t cause any issues at the moment.
I checked the cable issues on the forum and found that using only official cables is recommended. However, given the application, USB panel connectors are necessary.
Hi @jed-roboe,
Welcome to the Stereolabs forums ![]()
Indeed, in the general case we recommend using the official cables from Stereolabs as these have been tested and validated extensively with our cameras.
We do not have specific experience with using a repeater on USB A Male to Male cables, but I would suggest you try a cable with an active repeater as this usually solves USB reliability over larger distances.