A problem about installing SDK of zed 2i

Hi!
I met a error when installing the SDK 3.5.0。
my environment: cuda 10.2 ubuntu 18.04 package:ZED_SDK_Ubuntu18_cuda10.2_v3.5.0.run

The mistake shows:
The following packages have unsatisfied dependencies:
Libusb-1.0-0-dbg: dependency: libusb-1.0-0 (= 2:1.0.17-1ubuntu2), but 2:1.0.21-2 is about to be installed.

After that I install libusb-1.0-0=2:1.0.17-1ubuntu2 and libusb-1.0-0-dev, but it still shows this error. I don’t know how to solve it.
Thanks!

Hi @wildpig888
can you please provide more information (CPU, GPU, ecc) about the host system that you are using with the ZED2i?

Thank you

HI!
I tried at laptop, pc and nvidia board.

laptop and pc has the same problem. GPU is 1660ti and 1050ti, the driver is 440 and 460. Both of them are ubuntu 18.04, cuda10.2. CPU is intel i7 10th generation.

nvidia board is NVIDIA Xavier NX. the system is jetpack4.5.

THANKS.

Solved. Changing the sources of downloading.Thanks.