Hello, I’m quite new to Stereolabs and ROS.
So I have a basic question, how do I start a SVO recording when I run roslaunch zed_wrapper zed2i.launch in the first terminal?
And is it possible to start two recordings at the same time, because I have two ZEDs running parallel using the multicam example?
Hi @gpodann
you can start the SVO recoding by calling the start_svo_recording
service:
https://www.stereolabs.com/docs/ros/zed-node/#services
You can start it by command line or by using the Service Caller
plugin of the rqt
GUI tool.
Thanks for the link.
But what is the exact command line command to start it. I tried start_svo_recording and rosservice start_svo_recording but it didn’t work…
You can get the list of services with
$ rosservice list
then you can get the service info with
$ rosservice info /zed2i/zed_node/start_svo_recording
you can see that the only argument is the ROS filename, that must be an ABSOLUTE path name.
$ rosservice call /zed2i/zed_node/start_svo_recording "test.svo"
Hello!
Is it possible to record to the svo file only particular topics while using a ROS wrapper?
Or the solution is to convert svo to bag and extract desirable topics?
The SVO does not know what’s ROS.
The SVO is a file containing the RAW data stream from a ZED camera and it is used to “simulate” a connected device by opening it with the ZED SDK.
The ZED SDK uses the data provided by the SVO file in the same way it uses the data provided by a real connected camera.
When you set the SVO as an input for the ZED Wrapper, you start a ROS node that performs the same elaboration performed with a live camera, so you can choose which topic will be published simply by subscribing to it, in the same way, you do with a connected ZED.