platform: x86
cuda 11.4
ubuntu 18.04
- Cheese can display the camera.
- The tools of SDK can be executed correctly
- If I compile a sample, such as tutorials/tutorial 1 - hello ZED, the steps are as follows:
a. mkdir build && cd build
b. cmake …
c. make
the terminal will note:
make[2]: *** No rule to make target ‘/usr/lib/x86_64-linux-gnu/libusb-1.0.so’, needed by ‘ZED_Tutorial_1’. Stop.
CMakeFiles/Makefile2:67: recipe for target ‘CMakeFiles/ZED_Tutorial_1.dir/all’ failed
make[1]: *** [CMakeFiles/ZED_Tutorial_1.dir/all] Error 2
Makefile:83: recipe for target ‘all’ failed
make: *** [all] Error 2
While I checked the file libusb-1.0.so in /usr/lib/x86_64-linux-gnu:
/usr/lib/x86_64-linux-gnu$ ls -lh | grep libusb-1.0.so
lrwxrwxrwx 1 root root 29 3月 23 14:32 libusb-1.0.so → ./usr/local/lib/libusb-1.0.so - How can I solve this problem? thanks!
BTW, I just want to turn off the function of AWB.