[Streaming] Warning : receiving port 30000 is not available (already used)... switching to port 30002. Retrying... [Streaming] Warning : receiving port 30002 is not available (already used)... switching to port 30004. Retrying... [Streaming] No backward compatibility required. [Streaming] Warning: Corrupted frame chunk received (recv: 196 / expect 16100) from ip : 127.0.0.1 at ts 1762968789225(ms) Opening in BLOCKING MODE NvMMLiteOpen : Block : BlockType = 279 NvMMLiteBlockCreate : Block : BlockType = 279 Camera 316310960 connected successfully on port 30000 --- Camera 316310960 Information --- ZED Model : ZED XOne UHD ZED Serial Number : 316310960 ZED Firmware : 2001/0 ZED Resolution : 1920x1200 ZED FPS : 30 [Streaming] Warning : receiving port 30002 is not available (already used)... switching to port 30004. Retrying... [Streaming] Warning : receiving port 30004 is not available (already used)... switching to port 30006. Retrying... [Streaming] No backward compatibility required. Opening in BLOCKING MODE NvMMLiteOpen : Block : BlockType = 279 NvMMLiteBlockCreate : Block : BlockType = 279 Camera 310559220 connected successfully on port 30002 --- Camera 310559220 Information --- ZED Model : ZED XOne UHD ZED Serial Number : 310559220 ZED Firmware : 2001/0 ZED Resolution : 1920x1200 ZED FPS : 30 this is the 0'th image dropped this is the 0'th image dropped this is the 1'th image dropped this is the 1'th image dropped this is the 2'th image dropped this is the 2'th image dropped this is the 3'th image dropped this is the 3'th image dropped this is the 4'th image dropped this is the 4'th image dropped this is the 5'th image dropped this is the 5'th image dropped this is the 6'th image dropped this is the 6'th image dropped this is the 7'th image dropped this is the 8'th image dropped this is the 7'th image dropped this is the 9'th image dropped Camera 310559220 - Captured frame 10 this is the 8'th image dropped this is the 10'th image dropped this is the 11'th image dropped this is the 9'th image dropped Camera 316310960 - Captured frame 10 this is the 12'th image dropped this is the 10'th image dropped this is the 13'th image dropped this is the 14'th image dropped this is the 11'th image dropped this is the 15'th image dropped this is the 12'th image dropped this is the 16'th image dropped this is the 13'th image dropped this is the 17'th image dropped this is the 14'th image dropped this is the 18'th image dropped this is the 19'th image dropped Camera 310559220 - Captured frame 20 this is the 15'th image dropped this is the 20'th image dropped this is the 16'th image dropped this is the 21'th image dropped this is the 17'th image dropped this is the 22'th image dropped this is the 23'th image dropped this is the 18'th image dropped this is the 24'th image dropped this is the 19'th image dropped Camera 316310960 - Captured frame 20 this is the 25'th image dropped this is the 20'th image dropped this is the 26'th image dropped this is the 21'th image dropped this is the 27'th image dropped this is the 28'th image dropped this is the 22'th image dropped this is the 29'th image dropped Camera 310559220 - Captured frame 30 this is the 23'th image dropped this is the 30'th image dropped this is the 31'th image dropped this is the 24'th image dropped this is the 32'th image dropped this is the 25'th image dropped this is the 33'th image dropped this is the 26'th image dropped this is the 34'th image dropped this is the 35'th image dropped this is the 27'th image dropped this is the 36'th image dropped this is the 28'th image dropped this is the 37'th image dropped this is the 29'th image dropped Camera 316310960 - Captured frame 30 this is the 38'th image dropped this is the 39'th image dropped Camera 310559220 - Captured frame 40 this is the 30'th image dropped this is the 40'th image dropped this is the 31'th image dropped this is the 41'th image dropped this is the 42'th image dropped this is the 32'th image dropped this is the 43'th image dropped this is the 33'th image dropped this is the 44'th image dropped this is the 34'th image dropped this is the 45'th image dropped this is the 46'th image dropped this is the 35'th image dropped this is the 47'th image dropped this is the 36'th image dropped this is the 48'th image dropped this is the 37'th image dropped this is the 49'th image dropped Camera 310559220 - Captured frame 50 this is the 50'th image dropped this is the 38'th image dropped this is the 51'th image dropped this is the 39'th image dropped Camera 316310960 - Captured frame 40 this is the 52'th image dropped this is the 40'th image dropped this is the 53'th image dropped this is the 54'th image dropped this is the 41'th image dropped this is the 55'th image dropped this is the 42'th image dropped this is the 56'th image dropped this is the 43'th image dropped this is the 57'th image dropped this is the 58'th image dropped this is the 44'th image dropped this is the 59'th image dropped Camera 310559220 - Captured frame 60 this is the 45'th image dropped this is the 60'th image dropped this is the 46'th image dropped this is the 61'th image dropped this is the 62'th image dropped this is the 47'th image dropped this is the 63'th image dropped this is the 64'th image dropped this is the 48'th image dropped this is the 65'th image dropped this is the 49'th image dropped Camera 316310960 - Captured frame 50 this is the 66'th image dropped this is the 50'th image dropped this is the 67'th image dropped this is the 68'th image dropped this is the 51'th image dropped this is the 69'th image dropped Camera 310559220 - Captured frame 70 this is the 52'th image dropped this is the 70'th image dropped this is the 53'th image dropped this is the 71'th image dropped this is the 72'th image dropped this is the 54'th image dropped this is the 73'th image dropped this is the 55'th image dropped this is the 74'th image dropped this is the 75'th image dropped this is the 56'th image dropped this is the 76'th image dropped this is the 57'th image dropped this is the 77'th image dropped this is the 58'th image dropped this is the 78'th image dropped this is the 79'th image dropped Camera 310559220 - Captured frame 80 this is the 59'th image dropped Camera 316310960 - Captured frame 60 this is the 80'th image dropped this is the 60'th image dropped this is the 81'th image dropped this is the 61'th image dropped this is the 82'th image dropped this is the 62'th image dropped this is the 83'th image dropped this is the 84'th image dropped this is the 63'th image dropped this is the 85'th image dropped this is the 64'th image dropped this is the 86'th image dropped this is the 65'th image dropped this is the 87'th image dropped this is the 88'th image dropped this is the 66'th image dropped this is the 89'th image dropped Camera 310559220 - Captured frame 90 this is the 67'th image dropped this is the 90'th image dropped this is the 68'th image dropped this is the 91'th image dropped this is the 92'th image dropped this is the 69'th image dropped Camera 316310960 - Captured frame 70 this is the 93'th image dropped this is the 70'th image dropped this is the 94'th image dropped this is the 71'th image dropped this is the 95'th image dropped ^C Ctrl+C pressed. Exiting... Camera 316310960 - Closed Camera 310559220 - Closed Program exited successfully terminate called without an active exception Aborted (core dumped)