{
    "AI Models": {
        "info": [
            "MULTI CLASS DETECTION is not optimized",
            "MULTI CLASS MEDIUM DETECTION is not optimized",
            "MULTI CLASS ACCURATE DETECTION is not optimized",
            "HUMAN BODY FAST DETECTION is not optimized",
            "HUMAN BODY MEDIUM DETECTION is not optimized",
            "HUMAN BODY ACCURATE DETECTION is not optimized",
            "HUMAN BODY 38 FAST DETECTION is not optimized",
            "HUMAN BODY 38 MEDIUM DETECTION is not optimized",
            "HUMAN BODY 38 ACCURATE DETECTION is not optimized",
            "PERSON HEAD DETECTION is not optimized",
            "PERSON HEAD ACCURATE DETECTION is not optimized",
            "REID ASSOCIATION is not optimized",
            "NEURAL LIGHT DEPTH is not optimized",
            "NEURAL DEPTH is not optimized",
            "NEURAL PLUS DEPTH is not optimized"
        ]
    },
    "CUDA Operations": {
        "cudaDeviceCount": 1,
        "cudaDriverVersion": 13000,
        "cudaDriverVersionString": "13.0",
        "cudaGetDeviceCountResult": 0,
        "cudaRuntimeLoaded": true,
        "cudaRuntimeVersion": 13000,
        "cudaRuntimeVersionString": "13.0",
        "cudaTestVersion": "1.0",
        "gpuTests": [
            {
                "computeCapability": "12.1",
                "computeCapabilityMajor": 12,
                "computeCapabilityMinor": 1,
                "freeResult": 0,
                "freeSuccess": true,
                "gpuId": 0,
                "gpuName": "NVIDIA GB10",
                "mallocResult": 0,
                "mallocSuccess": true,
                "memcpyD2HResult": 0,
                "memcpyD2HSuccess": true,
                "memcpyH2DResult": 0,
                "memcpyH2DSuccess": true,
                "memoryBusWidthBits": 256,
                "memsetResult": 0,
                "memsetSuccess": true,
                "multiProcessorCount": 48,
                "pciBusId": 1,
                "pciDeviceId": 0,
                "pciDomainId": 15,
                "setDeviceResult": 0,
                "testElements": 1048576,
                "testPassed": true,
                "testSizeBytes": 4194304,
                "totalGlobalMemMB": 124546,
                "validationPassed": true
            }
        ],
        "testSizeMB": 1,
        "valid": [
            "<b>GPU 0 (NVIDIA GB10):</b> CUDA operations working correctly"
        ]
    },
    "Camera Test": {
        "CorruptedFirmware": [
        ],
        "InternalDevicesCount (GMSL)": [
        ],
        "InternalDevicesCount (USB)": [
        ],
        "USBList": [
            {
                "USB_path": "/2",
                "idProduct": "0x3630",
                "idVendor": "0x13d3"
            },
            {
                "USB_path": "/1",
                "idProduct": "0x0626",
                "idVendor": "0x05e3"
            },
            {
                "USB_path": "/1/2",
                "idProduct": "0xc53f",
                "idVendor": "0x046d"
            },
            {
                "USB_path": "/1/1",
                "idProduct": "0x0800",
                "idVendor": "0x045e"
            },
            {
                "USB_path": "/1",
                "idProduct": "0x0610",
                "idVendor": "0x05e3"
            }
        ],
        "ZEDCount": [
        ],
        "ZEDDetected": [
        ],
        "ZEDs": [
        ],
        "error": [
            "<b>No Camera detected</b> <br/> Make sure the camera is plugged in.",
            "<b>No Camera detected</b> <br/> Make sure the camera is plugged in."
        ],
        "notTested": [
            "Please connect a camera to test the USB connection.",
            "Please connect a camera to test the USB connection."
        ]
    },
    "Graphics Card": {
        "deviceCount": 1,
        "deviceDriverVersion": 13000,
        "devices": [
            {
                "arch": "Unknown Future Architecture",
                "computeCapability": "12.1",
                "cores": 0,
                "name": "NVIDIA GB10",
                "totalMemoryBytes": "130596732928",
                "totalMemoryMB": 124546.75
            }
        ],
        "glx_info": "OpenGL vendor string: NVIDIA Corporation\nOpenGL renderer string: NVIDIA GB10/PCIe\nOpenGL core profile version string: 4.6.0 NVIDIA 580.142\nOpenGL core profile shading language version string: 4.60 NVIDIA\nOpenGL core profile context flags: (none)\nOpenGL core profile profile mask: core profile\nOpenGL core profile extensions:\nOpenGL version string: 4.6.0 NVIDIA 580.142\nOpenGL shading language version string: 4.60 NVIDIA\nOpenGL context flags: (none)\nOpenGL profile mask: (none)\nOpenGL extensions:\nOpenGL ES profile version string: OpenGL ES 3.2 NVIDIA 580.142\nOpenGL ES profile shading language version string: OpenGL ES GLSL ES 3.20\nOpenGL ES profile extensions:\n",
        "initResult": 0,
        "valid": [
            "<b>Graphics card: </b> NVIDIA GB10"
        ]
    },
    "Processor": {
        "OS": "Ubuntu 24.04.4 LTS ",
        "avxSupported": false,
        "coreCount": "20100%",
        "cpu": "",
        "datetime": "2026-06-22 09:28:09 AM",
        "hyperThreading": "1",
        "motherboard": "038RY7, Dell Inc.",
        "platform": "ARM desktop (SBSA)",
        "ramCapacity": "130.596733",
        "ramUsage": "",
        "ramUsed": "13.170487",
        "threadCount": "221100",
        "valid": [
            "<b>Processor: </b> ",
            "<b>Motherboard: </b> 038RY7, Dell Inc."
        ]
    },
    "ZED SDK": {
        "CUDA Toolkit version": "V13.0.88 -->located in /usr/local/cuda-13.0/bin/nvcc",
        "CUDA loading": false,
        "GPU Driver Version": "Driver Version                                         : 580.142",
        "GPU Performance": "    Performance State                                  : P0",
        "ZED SDK Version (Diag)": "5.4.0",
        "ZED SDK Version (RT)": "5.4.0",
        "ai": {
            "checkAI": true,
            "cudaVersion": 13000,
            "tensorVersion": 101601
        },
        "binFiles": [
            "libsl_ai.so",
            "libsl_zed.so"
        ],
        "resourcesFiles": [
            "neural_depth_5.3.model",
            "neural_depth_light_5.3.model"
        ],
        "resourcesFilesExpected": [
            "objects_performance_3.2"
        ],
        "valid": [
            "<b>ZED SDK version:</b> 5.4.0",
            "<b>CUDA version:</b> V13.0.88"
        ]
    }
}