# ZedX Timestamps

**URL:** <https://community.stereolabs.com/t/zedx-timestamps/8924>\
**Category:** Software\
**Created:** [May 27, 2025, 5:58pm UTC](https://community.stereolabs.com/t/zedx-timestamps/8924 "2025-05-27T17:58:28Z")\
**Posts on this page:** 1\
**Showing post:** 23

<div class="post-metadata">

**Author:** ![Myzhar](https://community.stereolabs.com/user_avatar/community.stereolabs.com/myzhar/32/11_2.png) [@Myzhar](https://community.stereolabs.com/u/Myzhar)\
**Post date:** [November 13, 2026, 4:18pm UTC](https://community.stereolabs.com/t/zedx-timestamps/8924/23 "2026-11-13T16:18:38Z")

</div>

Hi @Parv-Maheshwari,

> [@Parv-Maheshwari](#):
>
> Unfortunately, since we are in the middle of a data collection campaign, upgrading our stack with new SDKs, drivers, etc., runs the risk of newer data not following the same distribution as the old, so upgrading is not possible right now.

Understood. The behavior described below also applies to your current setup. I still recommend upgrading once the campaign is over.

> [@Parv-Maheshwari](#):
>
> If I have a dropped trigger at T and I sent triggers at T-1 and T+1 in system time, will my corresponding dropped image be at T or T+1?

The dropped image is the one at T+1, which matches what you see in your data.

In slave mode, the camera does not start the exposure on the rising edge; it aligns the **end** of the exposure with the rising edge. Each rising edge is the reference used to schedule the next frame, whose exposure ends one trigger period later, on the following edge. This means:

- the edge at T-1 generates the image whose exposure ends at T, so its `IMAGE` timestamp is close to T;
- if the edge at T is missing, no frame is scheduled to end at T+1, so the image at T+1 is dropped.

> [@Parv-Maheshwari](#):
>
> Based on the ZEDX docs, which say that the camera syncs the start of exposure to the rise of an edge,

Our documentation says the rising edge is synchronized with the end of the exposure phase of the CMOS sensor: [ZED Link Quad GPIO Triggering](https://docs.stereolabs.com/docs/products/embedded/zed-link-capture-card/zed-link-quad/zed-link-quad-gpio-triggering). The slave-mode behavior is also covered in this thread: [Understanding Slave mode on the Quad capture card](https://community.stereolabs.com/t/understanding-slave-mode-on-the-quad-capture-card/10777). If you found a page that says the exposure _starts_ on the rising edge, please share the link so we can correct it.

This also explains your 31.76 ms measurement. If you pair each image with the edge that scheduled it (T-1), you get an offset of about one period. If you pair it with the edge it is aligned to (T), the `IMAGE` timestamp falls close to the end of the exposure.

---

_[View the full topic](https://community.stereolabs.com/t/zedx-timestamps/8924)._