ZedX Timestamps

Hi @Parv-Maheshwari,

Understood. The behavior described below also applies to your current setup. I still recommend upgrading once the campaign is over.

The dropped image is the one at T+1, which matches what you see in your data.

In slave mode, the camera does not start the exposure on the rising edge; it aligns the end of the exposure with the rising edge. Each rising edge is the reference used to schedule the next frame, whose exposure ends one trigger period later, on the following edge. This means:

  • the edge at T-1 generates the image whose exposure ends at T, so its IMAGE timestamp is close to T;
  • if the edge at T is missing, no frame is scheduled to end at T+1, so the image at T+1 is dropped.

Our documentation says the rising edge is synchronized with the end of the exposure phase of the CMOS sensor: ZED Link Quad GPIO Triggering. The slave-mode behavior is also covered in this thread: Understanding Slave mode on the Quad capture card. If you found a page that says the exposure starts on the rising edge, please share the link so we can correct it.

This also explains your 31.76 ms measurement. If you pair each image with the edge that scheduled it (T-1), you get an offset of about one period. If you pair it with the edge it is aligned to (T), the IMAGE timestamp falls close to the end of the exposure.