# ZEDX Camera with Scout Mini Integration on Jetson AGX Orin

**URL:** <https://community.stereolabs.com/t/zedx-camera-with-scout-mini-integration-on-jetson-agx-orin/9649>\
**Category:** ROS2\
**Tags:** python, jetson, ros2\
**Created:** [August 8, 2025, 7:34am UTC](https://community.stereolabs.com/t/zedx-camera-with-scout-mini-integration-on-jetson-agx-orin/9649 "2025-08-08T07:34:29Z")\
**Posts on this page:** 2\
**Page:** 1

<div class="post-metadata">

**Author:** ![doruk.sonmez](https://community.stereolabs.com/letter_avatar_proxy/v4/letter/d/67e7ee/32.png) [@doruk.sonmez](https://community.stereolabs.com/u/doruk.sonmez)\
**Post date:** [August 8, 2025, 7:34am UTC](https://community.stereolabs.com/t/zedx-camera-with-scout-mini-integration-on-jetson-agx-orin/9649/1 "2025-08-08T07:34:29Z")

</div>

Hi all,

I’m currently building an AMR based on ZEDX, S2 Lidar, and Scout Mini. So far, I have been able to integrate this stack with the slam\_toolbox and Nav2 packages. However, I’m not sure if my TF tree is correct.

 ![rviz](https://community.stereolabs.com/uploads/default/original/2X/d/d2b0e7bb365dfd15bf4d1603671163eb0a12e9f4.jpeg)

 ![tf_tree](https://community.stereolabs.com/uploads/default/original/2X/9/90608bc1e72d03c4120df79a7d55b7b07068c5bd.jpeg)

 ![image](https://community.stereolabs.com/uploads/default/original/2X/0/0de32285faa167f94cf9ce455f62807d50ab98f4.jpeg)

With this setup, it looks like I’m able to generate a 2D map. However, I’m wondering how I can benefit from the official ZEDX - Scout Mini Integration ( [ZED integration on a Robot - Stereolabs](https://www.stereolabs.com/docs/ros2/ros2-robot-integration) ). Additionally, there are two related topics, namely `/zed/zed_node/odom` and `/zed/zed_node/pose`, when I run the stereo node with: ``ros2 launch zed_wrapper zed_camera.launch.py camera_model:=zedx"`. How can these two be used for slam\_toolbox and Nav2 stacks? Are these meant for increasing the accuracy with VIO, as it is mentioned here: [Using VIO to Augment Robot Odometry — Nav2 1.0.0 documentation](https://docs.nav2.org/tutorials/docs/integrating_vio.html#using-vio-to-augment-robot-odometry) ?

---

<div class="post-metadata">

**Author:** ![mattrouss](https://community.stereolabs.com/user_avatar/community.stereolabs.com/mattrouss/32/2452_2.png) [@mattrouss](https://community.stereolabs.com/u/mattrouss)\
**Post date:** [August 11, 2025, 3:54pm UTC](https://community.stereolabs.com/t/zedx-camera-with-scout-mini-integration-on-jetson-agx-orin/9649/2 "2025-08-11T15:54:13Z")

</div>

Hi @doruk.sonmez,

If you wish to fuse odometry data using different sources, I would recommend following the tutorial from the Nav2 documentation: [Using VIO to Augment Robot Odometry — Nav2 1.0.0 documentation](https://docs.nav2.org/tutorials/docs/integrating_vio.html#setting-up-zed-ros)

And setting the following parameters in the zed\_ros\_wrapper config yaml:

```yaml
pos_tracking:
    publish_tf: false # Disables odom -> base_link TF transformation
    publish_map_tf: false # Disables map -> odom TF transformation, set this as false, nav2 documentation has a typo
    area_memory: false # Disables loop closure computation, but Pose topic for global VSLAM still published (but now pure VIO)

    # Optional optimizations
    two_d_mode: false # Or true, up to you!
    pos_tracking_enabled: true # of course!
    path_max_count: 30
    qos_depth: 5

```

This will allow using the `robot_localization` package to fuse the odometry from the ZED and from lidar and use slam\_toolbox as your slam source.