# ZedBox Mini Crashes

**URL:** <https://community.stereolabs.com/t/zedbox-mini-crashes/11428>\
**Category:** Hardware\
**Tags:** jetson\
**Created:** [June 10, 2026, 8:43am UTC](https://community.stereolabs.com/t/zedbox-mini-crashes/11428 "2026-06-10T08:43:49Z")\
**Posts on this page:** 4\
**Page:** 1

<div class="post-metadata">

**Author:** ![MM10](https://community.stereolabs.com/letter_avatar_proxy/v4/letter/m/439d5e/32.png) [@MM10](https://community.stereolabs.com/u/MM10)\
**Post date:** [June 10, 2026, 8:43am UTC](https://community.stereolabs.com/t/zedbox-mini-crashes/11428/1 "2026-06-10T08:43:49Z")

</div>

Hi, I’m using a ZedBox Mini NX 16GB to stream two Zed X mini GSML2 Kamera via Ethernet to a ROS2 Wrapper. Since a few days the Zedbox becomes unresponsive, no pings or anything else works and the power LED shuts off. The two green Lights at the ethernet port art flickering synchronously. When power cycling the device by removing the 12V it turns back on. Currently I’m using the RT Kernel. Is there any known issues like this or do i have a bad ZEDbox mini?

---

<div class="post-metadata">

**Author:** ![MM10](https://community.stereolabs.com/letter_avatar_proxy/v4/letter/m/439d5e/32.png) [@MM10](https://community.stereolabs.com/u/MM10)\
**Post date:** [June 10, 2026, 8:57am UTC](https://community.stereolabs.com/t/zedbox-mini-crashes/11428/2 "2026-06-10T08:57:59Z")

</div>

This is the /etc/nv\_tegra\_release

```auto
# R36 (release), REVISION: 4.7, GCID: 42132812, BOARD: generic, EABI: aarch64, DATE: Thu Sep 18 22:54:44 UTC 2025
# KERNEL_VARIANT: oot
TARGET_USERSPACE_LIB_DIR=nvidia
TARGET_USERSPACE_LIB_DIR_PATH=usr/lib/aarch64-linux-gnu/nvidia

```

I’m running the board in the power mode 1

```auto
sudo nvpmodel -q
NV Power Mode: 10W
1

```

---

<div class="post-metadata">

**Author:** ![mattrouss](https://community.stereolabs.com/user_avatar/community.stereolabs.com/mattrouss/32/2452_2.png) [@mattrouss](https://community.stereolabs.com/u/mattrouss)\
**Post date:** [June 12, 2026, 4:29pm UTC](https://community.stereolabs.com/t/zedbox-mini-crashes/11428/3 "2026-06-12T16:29:06Z")

</div>

Hi @MM10 , this is not something we’ve seen.

Does changing the power mode to a higher mode avoid this issue? Running multiple cameras with different ZED SDK algorithms may consume over the 10W.

---

<div class="post-metadata">

**Author:** ![MM10](https://community.stereolabs.com/letter_avatar_proxy/v4/letter/m/439d5e/32.png) [@MM10](https://community.stereolabs.com/u/MM10)\
**Post date:** [July 2, 2026, 8:01am UTC](https://community.stereolabs.com/t/zedbox-mini-crashes/11428/4 "2026-07-02T08:01:56Z")

</div>

Update: The DC Supply for the Zedbox went over a cable that had voltage drop. When the Zedbox was pulling power the voltage dropped below 11V, resulting in the Zedbox turning off.