# ZED2i Image Tearing and Inversion Issue at Left 1/3 Area (Neural Plus, ROS1, SDK 4)

**URL:** <https://community.stereolabs.com/t/zed2i-image-tearing-and-inversion-issue-at-left-1-3-area-neural-plus-ros1-sdk-4/9394>\
**Category:** ROS1\
**Tags:** sdk\
**Created:** [July 15, 2025, 1:25am UTC](https://community.stereolabs.com/t/zed2i-image-tearing-and-inversion-issue-at-left-1-3-area-neural-plus-ros1-sdk-4/9394 "2025-07-15T01:25:37Z")\
**Posts on this page:** 4\
**Page:** 1

<div class="post-metadata">

**Author:** ![MarkdDk](https://community.stereolabs.com/user_avatar/community.stereolabs.com/markddk/32/4431_2.png) [@MarkdDk](https://community.stereolabs.com/u/MarkdDk)\
**Post date:** [July 15, 2025, 1:25am UTC](https://community.stereolabs.com/t/zed2i-image-tearing-and-inversion-issue-at-left-1-3-area-neural-plus-ros1-sdk-4/9394/1 "2025-07-15T01:25:37Z")

</div>

Hello,

We are currently using two ZED2i cameras in a ROS1 + ZED SDK 4 environment and are experiencing an intermittent but critical issue.

* * *

### 🧩 Issue Description

Occasionally, the image appears **torn or inverted around the left 1/3 vertical region** of the frame, as shown in the attached image.  
This issue tends to occur more frequently during object detection tasks and is difficult to reproduce consistently. The affected region fluctuates within a **±15% range around the left 1/3 area** , making it harder to isolate the root cause.

As a workaround, we tested reducing the resolution to **HD720** , which seems to **reduce the frequency of the issue** , but **it still occurs occasionally**. Therefore, the problem is likely not fully resolved by lowering resolution alone.

* * *

### ⚙ System Setup

- **Cameras** : 2 × ZED2i
- **PC** : Ubuntu 20.04, NVIDIA RTX 4060
- **Connection** : USB 3.0 (5m C-to-A cable; USB-C on camera side, USB-A on PC)
- **SDK** : ZED SDK 4.x
- **ROS** : ROS1 (Noetic)
- **Camera Mode** : Neural Plus, Resolution: 2K (also tested HD720)

* * *

### ❓What We Are Looking For

- Is there any **known cause or workaround** for this kind of image tearing and inversion, especially under long USB cables or Neural/Neural Plus modes?
- Within the **ROS1 ecosystem** , is there a recommended approach to **detect and filter corrupted frames** (e.g., analyzing image continuity, histogram anomalies, or checksum mismatch)?
- Are there any **ZED SDK or USB reliability settings** we can tune to reduce this issue further?

We would greatly appreciate any insights or advice on how to prevent or filter out such corrupted frames during runtime.

 ![Untitled_](https://community.stereolabs.com/uploads/default/original/2X/b/b89ebf33152e2a99184ade0a171588af4026be4a.jpeg)  
 ![depth_tearing_combined_20250613_111001_new](https://community.stereolabs.com/uploads/default/original/2X/1/120403e3e2ba0a538edeed5a4230229f5c1d04f0.jpeg)

---

<div class="post-metadata">

**Author:** ![Myzhar](https://community.stereolabs.com/user_avatar/community.stereolabs.com/myzhar/32/11_2.png) [@Myzhar](https://community.stereolabs.com/u/Myzhar)\
**Post date:** [July 15, 2025, 10:18am UTC](https://community.stereolabs.com/t/zed2i-image-tearing-and-inversion-issue-at-left-1-3-area-neural-plus-ros1-sdk-4/9394/2 "2025-07-15T10:18:51Z")

</div>

> [@MarkdDk](#):
>
> Occasionally, the image appears **torn or inverted around the left 1/3 vertical region** of the frame, as shown in the attached image.

This issue has been discussed quite a few times on the forum, and there are plenty of conversations about it you can explore.  
The frame tearing is normally caused by a bad USB 3 connection or a CPU overload.

In your case, I noticed that you are using two 5m long USB3 cables:

- Are they connected to two separate USB 3 channels?
- Are the cables active or passive?
- Are you using USB 3 hubs?

> [@MarkdDk](#):
>
> Within the **ROS1 ecosystem** , is there a recommended approach to **detect and filter corrupted frames** (e.g., analyzing image continuity, histogram anomalies, or checksum mismatch)?

No, the frame quality check is available only with the ROS 2 Wrapper.  
We are no longer adding new features to the ROS Wrapper because ROS is now EOL.

---

<div class="post-metadata">

**Author:** ![MarkdDk](https://community.stereolabs.com/user_avatar/community.stereolabs.com/markddk/32/4431_2.png) [@MarkdDk](https://community.stereolabs.com/u/MarkdDk)\
**Post date:** [August 12, 2025, 6:23am UTC](https://community.stereolabs.com/t/zed2i-image-tearing-and-inversion-issue-at-left-1-3-area-neural-plus-ros1-sdk-4/9394/3 "2025-08-12T06:23:44Z")

</div>

Hello,

Thanks for your response. Regarding the **frame quality check** feature, I would like to know if the function for this is available in the **ROS 2 API GitHub repository**.

If it exists, could you please let me know the exact location (file path and function name) so that I can review the code and try to implement it myself in ROS 1?

Thank you in advance.

---

<div class="post-metadata">

**Author:** ![Myzhar](https://community.stereolabs.com/user_avatar/community.stereolabs.com/myzhar/32/11_2.png) [@Myzhar](https://community.stereolabs.com/u/Myzhar)\
**Post date:** [August 28, 2025, 8:32am UTC](https://community.stereolabs.com/t/zed2i-image-tearing-and-inversion-issue-at-left-1-3-area-neural-plus-ros1-sdk-4/9394/4 "2025-08-28T08:32:41Z")

</div>

Hi @MarkdDk

Yes, it’s available with the ZED ROS2 Wrapper:

> <https://github.com/stereolabs/zed-ros2-wrapper/blob/master/zed_components/src/zed_camera/src/zed_camera_component_main.cpp#L8529-L8562>