# ZED X One stereo\_calibration script is so slow, basically unusable

**URL:** <https://community.stereolabs.com/t/zed-x-one-stereo-calibration-script-is-so-slow-basically-unusable/9982>\
**Category:** Software\
**Created:** [September 24, 2025, 6:56pm UTC](https://community.stereolabs.com/t/zed-x-one-stereo-calibration-script-is-so-slow-basically-unusable/9982 "2025-09-24T18:56:51Z")\
**Posts on this page:** 6\
**Page:** 1

<div class="post-metadata">

**Author:** ![adinesh](https://community.stereolabs.com/letter_avatar_proxy/v4/letter/a/e495f1/32.png) [@adinesh](https://community.stereolabs.com/u/adinesh)\
**Post date:** [September 24, 2025, 6:56pm UTC](https://community.stereolabs.com/t/zed-x-one-stereo-calibration-script-is-so-slow-basically-unusable/9982/1 "2025-09-24T18:56:51Z")

</div>

I’m following the procedure [here](https://github.com/stereolabs/zedx-one-capture/tree/main/stereo_calibration). im using ./zedx\_one\_stereo\_calibration. when I hit s to save the current frame, it seems like the application crashes out or is just so slow that the real time viewer doesn’t update anymore. has anyone else had this issue? im running on a jetson orin nx, and it isnt heating up excessively, so i should have the compute to do the simple task.

---

<div class="post-metadata">

**Author:** ![Myzhar](https://community.stereolabs.com/user_avatar/community.stereolabs.com/myzhar/32/11_2.png) [@Myzhar](https://community.stereolabs.com/u/Myzhar)\
**Post date:** [September 25, 2025, 8:17am UTC](https://community.stereolabs.com/t/zed-x-one-stereo-calibration-script-is-so-slow-basically-unusable/9982/3 "2025-09-25T08:17:35Z")

</div>

Hi @adinesh  
Have you configured the example to match the features of your calibration board?  
What you describe is normally caused by the code not detecting the board.

Please send a picture of the board that you are using and the settings.

---

<div class="post-metadata">

**Author:** ![adinesh](https://community.stereolabs.com/letter_avatar_proxy/v4/letter/a/e495f1/32.png) [@adinesh](https://community.stereolabs.com/u/adinesh)\
**Post date:** [September 25, 2025, 4:38pm UTC](https://community.stereolabs.com/t/zed-x-one-stereo-calibration-script-is-so-slow-basically-unusable/9982/4 "2025-09-25T16:38:20Z")

</div>

Sure!

 ![IMG_3985.HEIC](https://community.stereolabs.com/uploads/default/original/2X/9/9c355c7ccf7c181581b003c8e4c5cfba065c0ed7.jpeg)

I can see in the real time viewer that \>80% of the points are being found (looks close to 100%). My settings are:

int target\_w = 11; // number of horizontal inner edges

int target\_h = 9; // number of vertical inner edges

float square\_size = 86.0; // mm

The slowness is mostly when I click ‘s’, it takes 3 minutes (timed) for those images to save (as showed in the terminal output). About halfway through the coverage process, I keep getting prompts that the “Application is not Responding”, but if I wait long enough, that does go away. So far, if I wait long enough, it ends up being ok.

---

<div class="post-metadata">

**Author:** ![Myzhar](https://community.stereolabs.com/user_avatar/community.stereolabs.com/myzhar/32/11_2.png) [@Myzhar](https://community.stereolabs.com/u/Myzhar)\
**Post date:** [September 25, 2025, 5:48pm UTC](https://community.stereolabs.com/t/zed-x-one-stereo-calibration-script-is-so-slow-basically-unusable/9982/5 "2025-09-25T17:48:08Z")

</div>

> [@adinesh](#):
>
> int target\_w = 11; // number of horizontal inner edges
> 
> int target\_h = 9; // number of vertical inner edges
> 
> float square\_size = 86.0; // mm

Calibration parameters look correct.

> [@adinesh](#):
>
> The slowness is mostly when I click ‘s’, it takes 3 minutes (timed) for those images to save (as showed in the terminal output). About halfway through the coverage process, I keep getting prompts that the “Application is not Responding”, but if I wait long enough, that does go away. So far, if I wait long enough, it ends up being ok.

What NVIDIA Jetson module are you using? Is the power mode set to MAXN, and the `jetson_clocks.sh` script running?

---

<div class="post-metadata">

**Author:** ![adinesh](https://community.stereolabs.com/letter_avatar_proxy/v4/letter/a/e495f1/32.png) [@adinesh](https://community.stereolabs.com/u/adinesh)\
**Post date:** [September 25, 2025, 10:57pm UTC](https://community.stereolabs.com/t/zed-x-one-stereo-calibration-script-is-so-slow-basically-unusable/9982/6 "2025-09-25T22:57:06Z")

</div>

The power mode is set to MAXN\_SUPER (checked via `sudo jetson_clocks --show`), and I have run `sudo jetson_clocks`. Let me know if either of those aren’t correct.

This is the jetson board i have ([https://arkelectron.com/product/ark-just-a-jetson/?srsltid=AfmBOooyuHyCal7qWd\_-hrmiBZtSH5tF-yzm6GsNQIGRyC7ng8Q6W6ML](https://arkelectron.com/product/ark-just-a-jetson/?srsltid=AfmBOooyuHyCal7qWd_-hrmiBZtSH5tF-yzm6GsNQIGRyC7ng8Q6W6ML)) - it’s a Jetson Orin NX.

---

<div class="post-metadata">

**Author:** ![Myzhar](https://community.stereolabs.com/user_avatar/community.stereolabs.com/myzhar/32/11_2.png) [@Myzhar](https://community.stereolabs.com/u/Myzhar)\
**Post date:** [September 26, 2025, 1:28pm UTC](https://community.stereolabs.com/t/zed-x-one-stereo-calibration-script-is-so-slow-basically-unusable/9982/7 "2025-09-26T13:28:48Z")

</div>

What resolution are you using?

> [@adinesh](#):
>
> This is the Jetson board i have ([ARK Just A Jetson – ARK Electronics](https://arkelectron.com/product/ark-just-a-jetson/?srsltid=AfmBOooyuHyCal7qWd_-hrmiBZtSH5tF-yzm6GsNQIGRyC7ng8Q6W6ML)) - it’s a Jetson Orin NX.

Interesting. This board is not officially supported by the ZED X Driver; it’s nice to know it works with it with no modifications.