# ZED X One S - GMSL driver error & CAMERA STREAM FAILED TO START (Jetson Orin Nano)

**URL:** <https://community.stereolabs.com/t/zed-x-one-s-gmsl-driver-error-camera-stream-failed-to-start-jetson-orin-nano/10829>\
**Category:** ZED X\
**Tags:** jetson\
**Created:** [February 19, 2026, 8:42am UTC](https://community.stereolabs.com/t/zed-x-one-s-gmsl-driver-error-camera-stream-failed-to-start-jetson-orin-nano/10829 "2026-02-19T08:42:17Z")\
**Posts on this page:** 20\
**Page:** 1

<div class="post-metadata">

**Author:** ![NivC](https://community.stereolabs.com/letter_avatar_proxy/v4/letter/n/ecae2f/32.png) [@NivC](https://community.stereolabs.com/u/NivC)\
**Post date:** [February 19, 2026, 8:42am UTC](https://community.stereolabs.com/t/zed-x-one-s-gmsl-driver-error-camera-stream-failed-to-start-jetson-orin-nano/10829/1 "2026-02-19T08:42:17Z")

</div>

Hello [Stereolabs](https://www.stereolabs.com/) Support Team,

I am experiencing a streaming issue with my ZED setup and would appreciate your assistance.

**Hardware setup:**

- Jetson Orin Nano Development Kit

- ZED Link Capture Card Duo

- GMSL2 1–4 M-F cable

- 2x ZED X One S cameras

**Behavior observed:**

- In ZED Explorer, both cameras are detected successfully.

- I can see live frames from both cameras.

- However, when running ZED Diagnostics, I receive the following error under the GMSL DRIVER section:

“No camera stream  
Unable to establish a proper stream. Please reboot the device. If the problem persists, contact [Stereolabs](https://www.stereolabs.com/) support.”

- Occasionally after rebooting the Jetson device, the GMSL DRIVER shows a green check mark (✓), but i still having error on the cpp tutorial.

[ZED][ERROR] CAMERA STREAM FAILED TO START in sl::ERROR\_CODE sl:📷:open(sl::InitParameters)

**Troubleshooting steps already attempted:**

- Rebooted the Jetson multiple times.

- Switched between the GMSL2 ports.

- Tested both cameras individually.

- Issue persists.

It is confusing because ZED Explorer is able to display frames, yet the SDK fails to start the camera stream in C++ examples.  
note that i installed the GMSL2 Driver for my jetson orin JP 6.2.

I am attaching the ZED Diagnostic JSON file for your review.

Thank you very much for your support.

Best regards,  
Niv

**Update:**

Hello again,

I would like to provide an update regarding the issue.

I have uploaded a new ZED Diagnostic JSON file. The diagnostic tool now passes all the requirements, and no errors are reported in the GMSL DRIVER section.

However, the C++ tutorial still fails with the same error:

```auto
[ZED][ERROR] CAMERA STREAM FAILED TO START in sl::ERROR_CODE sl::open(sl::InitParameters)

```

After reviewing the system information, I noticed a potential version mismatch:

- My **L4T version** : `36.4.7`

- Installed **GMSL driver version** : `L4T 36.4`

I suspect the issue might be related to this version difference.

Could you please confirm whether L4T 36.4.7 is fully compatible with the L4T 36.4 GMSL driver?  
If not, should I downgrade or install a specific driver version?

Thank you again for your support.

Best regards,  
Niv

[ZED\_Diagnostic\_Results.json](https://community.stereolabs.com/uploads/short-url/c6QQym5sHYE98CcKA2r6iW91bKh.json) (19.8 KB)

---

<div class="post-metadata">

**Author:** ![Myzhar](https://community.stereolabs.com/user_avatar/community.stereolabs.com/myzhar/32/11_2.png) [@Myzhar](https://community.stereolabs.com/u/Myzhar)\
**Post date:** [February 19, 2026, 3:15pm UTC](https://community.stereolabs.com/t/zed-x-one-s-gmsl-driver-error-camera-stream-failed-to-start-jetson-orin-nano/10829/2 "2026-02-19T15:15:32Z")

</div>

Hi @NivC  
The diagnostic report is not complete.

Please run the commands with sudo:  
`sudo ZED_Diagnostic -c`  
`sudo ZED_Diagnostic --dmesg`

Send the two generated files.

---

<div class="post-metadata">

**Author:** ![NivC](https://community.stereolabs.com/letter_avatar_proxy/v4/letter/n/ecae2f/32.png) [@NivC](https://community.stereolabs.com/u/NivC)\
**Post date:** [February 19, 2026, 3:31pm UTC](https://community.stereolabs.com/t/zed-x-one-s-gmsl-driver-error-camera-stream-failed-to-start-jetson-orin-nano/10829/3 "2026-02-19T15:31:23Z")

</div>

I will do it on Sunday when I get back to office, but from the update of my message you can see the the versions, do you know if it should be compatible?

---

<div class="post-metadata">

**Author:** ![Myzhar](https://community.stereolabs.com/user_avatar/community.stereolabs.com/myzhar/32/11_2.png) [@Myzhar](https://community.stereolabs.com/u/Myzhar)\
**Post date:** [February 19, 2026, 3:42pm UTC](https://community.stereolabs.com/t/zed-x-one-s-gmsl-driver-error-camera-stream-failed-to-start-jetson-orin-nano/10829/4 "2026-02-19T15:42:27Z")

</div>

L4T v36.4.7 is supported.

If you recently updated the Jetson using the command `sudo apt upgrade` you could need to reinstall the driver.

If you get errors while installing the driver, please refer to this troubleshooting guide:

> **[Error: “Package nvidia-l4t-kernel is not configured yet” while installing the......](https://www.stereolabs.com/docs/embedded/zed-box-mini/troubleshooting#error-package-nvidia-l4t-kernel-is-not-configured-yet-while-installing-the-zed-x-driver)**
>
> ZED Box Mini not booting # If your ZED Box Mini does not turn on after a shutdown, follow these steps to diagnose the issue.

**Note** : the guide refers to the ZED Box device, but it’s valid for generic Jetson devkits too.

---

<div class="post-metadata">

**Author:** ![NivC](https://community.stereolabs.com/letter_avatar_proxy/v4/letter/n/ecae2f/32.png) [@NivC](https://community.stereolabs.com/u/NivC)\
**Post date:** [February 22, 2026, 8:02am UTC](https://community.stereolabs.com/t/zed-x-one-s-gmsl-driver-error-camera-stream-failed-to-start-jetson-orin-nano/10829/5 "2026-02-22T08:02:21Z")

</div>

Hey, here is the full diagnostic report as you asked:

[ZED\_Diagnostic\_Results.json](https://community.stereolabs.com/uploads/short-url/4vlxj2xe7cYW8blaGpfYwMf3s6r.json) (23.2 KB)

[dmesg.log](https://community.stereolabs.com/uploads/short-url/odk0AFJWocPmD2Zf0X66iLA2wKN.log) (14.6 KB)

i also had this output for `sudo ZED_Diagnostic --dmesg:`  
sudo ZED\_Diagnostic --dmesg

\*\* Please wait for completion… This might take up to 1 minute \*\*  
[2026-02-22 09:57:54.454] [ERROR] [ArgusCamera.cpp:440] [ZED-Argus][Critical] No current CUDA context available; cannot proceed without a valid context.  
[2026-02-22 09:57:56.105] [ERROR] [ArgusCamera.cpp:440] [ZED-Argus][Critical] No current CUDA context available; cannot proceed without a valid context.  
[2026-02-22 09:57:56.408] [ERROR] [ArgusCamera.cpp:440] [ZED-Argus][Critical] No current CUDA context available; cannot proceed without a valid context.  
[2026-02-22 09:57:56.718] [ERROR] [ArgusCamera.cpp:440] [ZED-Argus][Critical] No current CUDA context available; cannot proceed without a valid context.

- Running GMSL DRIVER Diagnostic : OK
- Running Log Kernel Trace (for ZED X) Diagnostic : OK

---

<div class="post-metadata">

**Author:** ![Myzhar](https://community.stereolabs.com/user_avatar/community.stereolabs.com/myzhar/32/11_2.png) [@Myzhar](https://community.stereolabs.com/u/Myzhar)\
**Post date:** [February 23, 2026, 4:43pm UTC](https://community.stereolabs.com/t/zed-x-one-s-gmsl-driver-error-camera-stream-failed-to-start-jetson-orin-nano/10829/6 "2026-02-23T16:43:38Z")

</div>

Hi @NivC  
are you working in headless mode, with no connected display?

If that’s the case, I recommend you follow the instructions [on this page](https://support.stereolabs.com/hc/en-us/articles/28103346502167-Why-can-t-I-use-the-ZED-X-camera-with-ssh-X-in-headless-mode).

---

<div class="post-metadata">

**Author:** ![NivC](https://community.stereolabs.com/letter_avatar_proxy/v4/letter/n/ecae2f/32.png) [@NivC](https://community.stereolabs.com/u/NivC)\
**Post date:** [February 23, 2026, 5:02pm UTC](https://community.stereolabs.com/t/zed-x-one-s-gmsl-driver-error-camera-stream-failed-to-start-jetson-orin-nano/10829/7 "2026-02-23T17:02:02Z")

</div>

Hey, I am working on jetson orin nano i connected to display via display port cable.

---

<div class="post-metadata">

**Author:** ![Myzhar](https://community.stereolabs.com/user_avatar/community.stereolabs.com/myzhar/32/11_2.png) [@Myzhar](https://community.stereolabs.com/u/Myzhar)\
**Post date:** [February 23, 2026, 5:08pm UTC](https://community.stereolabs.com/t/zed-x-one-s-gmsl-driver-error-camera-stream-failed-to-start-jetson-orin-nano/10829/8 "2026-02-23T17:08:37Z")

</div>

Have you tried to execute the [ZED SDK tools](https://www.stereolabs.com/docs/development/zed-tools)?  
`ZED_Studio`  
`ZED_Explorer`  
`ZED_Depth_Viewer`

What is the output of the command `ZED_Explorer -a`?

---

<div class="post-metadata">

**Author:** ![NivC](https://community.stereolabs.com/letter_avatar_proxy/v4/letter/n/ecae2f/32.png) [@NivC](https://community.stereolabs.com/u/NivC)\
**Post date:** [February 23, 2026, 5:44pm UTC](https://community.stereolabs.com/t/zed-x-one-s-gmsl-driver-error-camera-stream-failed-to-start-jetson-orin-nano/10829/9 "2026-02-23T17:44:24Z")

</div>

`ZED_Studio and ZED_Explorer` are working and open my cameras, in the configuration I can’t use the depth view.

`ZED_Depth_Viewer` is not find the cameras.

---

<div class="post-metadata">

**Author:** ![Myzhar](https://community.stereolabs.com/user_avatar/community.stereolabs.com/myzhar/32/11_2.png) [@Myzhar](https://community.stereolabs.com/u/Myzhar)\
**Post date:** [February 23, 2026, 5:46pm UTC](https://community.stereolabs.com/t/zed-x-one-s-gmsl-driver-error-camera-stream-failed-to-start-jetson-orin-nano/10829/10 "2026-02-23T17:46:42Z")

</div>

> [@NivC](#):
>
> `ZED_Depth_Viewer` is not find the cameras.

This is expected. You are using a monocular camera, to use ZED Depth Viewer you need a stereo camera.  
You can realize a virtual stereo camera by coupling two ZED X One S cameras:

> **[Setting up the ZED X One Stereo - Stereolabs](https://www.stereolabs.com/docs/cameras/zed-x-one/zed-x-one-stereo)**
>
> Two ZED X One cameras can be combined to create a Virtual Stereo Vision system, functioning as a single stereoscopic camera similar to the ZED 2i or ZED X.

---

<div class="post-metadata">

**Author:** ![NivC](https://community.stereolabs.com/letter_avatar_proxy/v4/letter/n/ecae2f/32.png) [@NivC](https://community.stereolabs.com/u/NivC)\
**Post date:** [February 23, 2026, 5:51pm UTC](https://community.stereolabs.com/t/zed-x-one-s-gmsl-driver-error-camera-stream-failed-to-start-jetson-orin-nano/10829/11 "2026-02-23T17:51:53Z")

</div>

> [@Myzhar](#):
>
> monocular camera, to use ZED Depth Viewer you need a stereo camera.  
> You can realize a virtual stereo camera by coupling two ZED X One S cameras:

Ok i sm using 2 ZED X One S narrow cameras, but what about the code I cannot compile, for example in the tutorials folder when i try to compile the first tutorial:”[tutorial 1 - hello ZE](https://github.com/stereolabs/zed-sdk/tree/master/tutorials/tutorial%201%20-%20hello%20ZED)D” , I got this error:  
[ZED][ERROR] CAMERA STREAM FAILED TO START in sl::ERROR\_CODE sl:📷:open(sl::InitParameters)

The reason of it it’s because of the fact I am using 2 ZED X One S cameras with capture card link, and i this code is not suitable for me?

I also tried to open the ZED Calibration, and it was crash every time i was start the process.

---

<div class="post-metadata">

**Author:** ![NivC](https://community.stereolabs.com/letter_avatar_proxy/v4/letter/n/ecae2f/32.png) [@NivC](https://community.stereolabs.com/u/NivC)\
**Post date:** [February 24, 2026, 7:39am UTC](https://community.stereolabs.com/t/zed-x-one-s-gmsl-driver-error-camera-stream-failed-to-start-jetson-orin-nano/10829/12 "2026-02-24T07:39:23Z")

</div>

More information about the problem:  
when running ZED\_Explorer -a i got this output:  
lps@lps:/usr/local/zed/tools$ ZED\_Explorer -a

## Cam 0

Model : “ZED XOne GS”  
S/N : 305416482  
State : “AVAILABLE”  
Path : /dev/i2c-9  
ID : 0  
Port : 0  
Type : “GMSL”

* * *

## Cam 1

Model : “ZED XOne GS”  
S/N : 306714912  
State : “AVAILABLE”  
Path : /dev/i2c-10  
ID : 1  
Port : 2  
Type : “GMSL”

* * *

I also tried to run the virtual stereo, the output i received:

./ZED\_Virtual\_Stereo\_Camera\_Control 305416482 306714912 111323474

- ZED One camera: ZED XOne GS (ID : 0, Serial: 305416482)
- ZED One camera: ZED XOne GS (ID : 1, Serial: 306714912)  
[Sample] Using Virtual Stereo from Serial Numbers: 305416482, 306714912 with virtual SN: 111323474  
[2026-02-24 09:34:57 UTC][ZED][INFO] Logging level INFO  
[2026-02-24 09:34:57 UTC][ZED][INFO] Using GMSL input… Switched to default resolution HD1200  
[2026-02-24 09:34:59 UTC][ZED][INFO] [Init] Camera FW version: 2001  
[2026-02-24 09:34:59 UTC][ZED][INFO] [Init] Video mode: HD1200@30  
[2026-02-24 09:34:59 UTC][ZED][INFO] [Init] Serial Number: S/N 111323474  
[2026-02-24 09:34:59 UTC][ZED][INFO] [Init] Failed to load a valid camera calibration. Opening the camera in uncalibrated mode. Depth and most modules will be disabled; only recording, streaming, and unrectified images are available. Please contact support if this persists.  
[2026-02-24 09:34:59 UTC][ZED][INFO] [Init] Depth mode selected: NONE. Ensure this mode matches your application’s performance and accuracy requirements. See [Depth Modes - Stereolabs](https://www.stereolabs.com/docs/depth-sensing/depth-modes) for help.  
[2026-02-24 09:34:59 UTC][ZED][ERROR] INVALID CALIBRATION FILE in sl::ERROR\_CODE sl:📷:open(sl::InitParameters)  
WARNING: Virtual Stereo rig not calibrated, only unrectified images and recording are available

ZED Model : Virtual ZED-X  
ZED Serial Number : 111323474  
ZED Camera Firmware : 2001/1000  
ZED Camera Resolution : 1920x1200  
ZED Camera FPS : 0

Camera controls hotkeys:

- Increase camera settings value: ‘+’
- Decrease camera settings value: ‘-’
- Toggle camera settings: ‘s’
- Toggle camera LED: ‘l’ (lower L)
- Reset all parameters: ‘r’
- Reset exposure ROI to full image ‘f’
- Use mouse to select an image area to apply exposure (press ‘a’)
- Exit : ‘q’

[Sample] Switch to camera settings: CONTRAST  
Segmentation fault (core dumped)

---

<div class="post-metadata">

**Author:** ![Myzhar](https://community.stereolabs.com/user_avatar/community.stereolabs.com/myzhar/32/11_2.png) [@Myzhar](https://community.stereolabs.com/u/Myzhar)\
**Post date:** [February 24, 2026, 9:17am UTC](https://community.stereolabs.com/t/zed-x-one-s-gmsl-driver-error-camera-stream-failed-to-start-jetson-orin-nano/10829/14 "2026-02-24T09:17:07Z")

</div>

> [@NivC](#):
>
> for example in the tutorials folder when i try to compile the first tutorial:”[tutorial 1 - hello ZE](https://github.com/stereolabs/zed-sdk/tree/master/tutorials/tutorial%201%20-%20hello%20ZED)D” , I got this error:  
> [ZED][ERROR] CAMERA STREAM FAILED TO START in sl::ERROR\_CODE sl:📷:open(sl::InitParameters)

This is because you are using the `sl::Camera` object with a monocular camera that requires the use of the `sl::CameraOne` object.

You must use the examples in this folder:

> **[zed-sdk/zed one at master · stereolabs/zed-sdk](https://github.com/stereolabs/zed-sdk/tree/master/zed%20one)**
>
> ⚡️The spatial perception framework for rapidly building smart robots and spaces - stereolabs/zed-sdk

> [@NivC](#):
>
> [2026-02-24 09:34:59 UTC][ZED][INFO] [Init] Failed to load a valid camera calibration. Opening the camera in uncalibrated mode. Depth and most modules will be disabled; only recording, streaming, and unrectified images are available. Please contact support if this persists.

Please follow the instructions in the documentation to learn how to configure and calibrate a virtual stereo camera before using it

> **[Setting up the ZED X One Stereo - Stereolabs](https://www.stereolabs.com/docs/cameras/zed-x-one/zed-x-one-stereo)**
>
> Two ZED X One cameras can be combined to create a Virtual Stereo Vision system, functioning as a single stereoscopic camera similar to the ZED 2i or ZED X.

---

<div class="post-metadata">

**Author:** ![Myzhar](https://community.stereolabs.com/user_avatar/community.stereolabs.com/myzhar/32/11_2.png) [@Myzhar](https://community.stereolabs.com/u/Myzhar)\
**Post date:** [February 24, 2026, 9:18am UTC](https://community.stereolabs.com/t/zed-x-one-s-gmsl-driver-error-camera-stream-failed-to-start-jetson-orin-nano/10829/15 "2026-02-24T09:18:32Z")

</div>

> [@enunes](#):
>
> We are experiencing similar issues since updating to SDK 5.2 and driver 1.4.0-LI-MAX96712-ZEDBOX-L4T36.4.0 when trying to grab 4K frames. We running the ZED One X 4k camera connected to a ZED box Jetson Orin Nano using GSML2. Here is our output for ZED\_Explorer -a

Hi @enunes  
This is a different problem. Please do not reply to a thread with different support requests.  
It’s best practice to create a new discussion thread, and eventually link existing threads if you think they are relevant to the discussion.

---

<div class="post-metadata">

**Author:** ![enunes](https://community.stereolabs.com/user_avatar/community.stereolabs.com/enunes/32/5245_2.png) [@enunes](https://community.stereolabs.com/u/enunes)\
**Post date:** [February 24, 2026, 9:42am UTC](https://community.stereolabs.com/t/zed-x-one-s-gmsl-driver-error-camera-stream-failed-to-start-jetson-orin-nano/10829/16 "2026-02-24T09:42:54Z")

</div>

@Myzhar Thanks for the response, and sorry about that. I deleted my post, and will open a thread

---

<div class="post-metadata">

**Author:** ![NivC](https://community.stereolabs.com/letter_avatar_proxy/v4/letter/n/ecae2f/32.png) [@NivC](https://community.stereolabs.com/u/NivC)\
**Post date:** [February 24, 2026, 12:39pm UTC](https://community.stereolabs.com/t/zed-x-one-s-gmsl-driver-error-camera-stream-failed-to-start-jetson-orin-nano/10829/17 "2026-02-24T12:39:29Z")

</div>

i was trying to calibrate the cameras using this guidance, but again i have this issue:

**Terminal line:**  
$/zed-opencv-calibration/build/stereo\_calibration$ ./zed\_stereo\_calibration --virtual --left\_sn 305416482 --right\_sn 306714912 --h\_edges 11 --v\_edges 8 --square\_size 65.3

## Inserting my calibration board information.

**output:**  
\*\*\* Stereo Camera Calibration Tool \*\*\*

The calibration process requires a checkerboard of known characteristics.

- Expected checkerboard features:

- Lens distorsion model: Radial-Tangential

- Virtual Stereo Camera mode enabled.

- Using serial numbers for left and right cameras: 305416482, 306714912

- Unique Virtual SN: 111323474 (Generated by the ZED SDK)

- ZED X One GS Virtual Stereo Camera detected.

- Camera Model: Virtual ZED-X

- Camera Serial Number: 111323474

- Camera Resolution: 1920 x 1200

- Using prior calibration: No  
**Segmentation fault (core dumped)**

after that it crashed immediately.

2.Using 2 ZED X One monocular cameras , i need to use **virtual** for the calibration?  
what that Virtual meaning ?

---

<div class="post-metadata">

**Author:** ![Myzhar](https://community.stereolabs.com/user_avatar/community.stereolabs.com/myzhar/32/11_2.png) [@Myzhar](https://community.stereolabs.com/u/Myzhar)\
**Post date:** [February 24, 2026, 4:27pm UTC](https://community.stereolabs.com/t/zed-x-one-s-gmsl-driver-error-camera-stream-failed-to-start-jetson-orin-nano/10829/18 "2026-02-24T16:27:39Z")

</div>

> [@NivC](#):
>
> Using 2 ZED X One monocular cameras , i need to use **virtual** for the calibration?  
> what that Virtual meaning ?

“Virtual” means that you are creating a stereo camera by composing two monocular cameras; you are not using a “Real” ZED Stereo Camera.

> [@NivC](#):
>
> Segmentation fault (core dumped)

It’s not possible to understand the cause of the crash without information.  
Have you tried to debug the code to understand at what line the crash happens?

---

<div class="post-metadata">

**Author:** ![NivC](https://community.stereolabs.com/letter_avatar_proxy/v4/letter/n/ecae2f/32.png) [@NivC](https://community.stereolabs.com/u/NivC)\
**Post date:** [February 25, 2026, 1:46pm UTC](https://community.stereolabs.com/t/zed-x-one-s-gmsl-driver-error-camera-stream-failed-to-start-jetson-orin-nano/10829/19 "2026-02-25T13:46:58Z")

</div>

> It’s not possible to understand the cause of the crash without information.  
> Have you tried to debug the code to understand at what line the crash happens?

 ![image](https://community.stereolabs.com/uploads/default/original/2X/d/d58fde6ad5385b583bc0a6dff6d42c0bfe647f52.png)

 ![image](https://community.stereolabs.com/uploads/default/original/2X/5/519520ed9ceac305fb39ddb56e76b4d1a714c5ce.png)

 ![image](https://community.stereolabs.com/uploads/default/original/2X/3/3624ddc092d22daa1b85c16dd0b998f77cd07fd1.png)

---

<div class="post-metadata">

**Author:** ![Myzhar](https://community.stereolabs.com/user_avatar/community.stereolabs.com/myzhar/32/11_2.png) [@Myzhar](https://community.stereolabs.com/u/Myzhar)\
**Post date:** [February 25, 2026, 1:54pm UTC](https://community.stereolabs.com/t/zed-x-one-s-gmsl-driver-error-camera-stream-failed-to-start-jetson-orin-nano/10829/20 "2026-02-25T13:54:07Z")

</div>

> [@NivC](#):
>
> ./zed\_stereo\_calibration --virtual --left\_sn 305416482 --right\_sn 306714912 --h\_edges 11 --v\_edges 8 --square\_size 65.3

What’s the output of the command `ZED_Explorer -a`?

---

<div class="post-metadata">

**Author:** ![NivC](https://community.stereolabs.com/letter_avatar_proxy/v4/letter/n/ecae2f/32.png) [@NivC](https://community.stereolabs.com/u/NivC)\
**Post date:** [February 25, 2026, 2:01pm UTC](https://community.stereolabs.com/t/zed-x-one-s-gmsl-driver-error-camera-stream-failed-to-start-jetson-orin-nano/10829/21 "2026-02-25T14:01:25Z")

</div>

![image](https://community.stereolabs.com/uploads/default/original/2X/4/42b1ba9f9709eb62401011ccf409afdeeb775a70.png)\

[Next page](https://community.stereolabs.com/t/zed-x-one-s-gmsl-driver-error-camera-stream-failed-to-start-jetson-orin-nano/10829.md?page=2)